This is an old revision of the document!
AD2430
Evaluation boards
The Evaluation boards used in the AD2430 demos are explained in the following subsections.
EVAL-AD2430WD1BZ
Figure 14 shows an EVAL-AD2430WD1BZ board which can be used as either an A2B main or sub node. The board has following components
AD2430 A2B transceiver
ADAU1452 SigmaDSP Audio Processor
512K Self-Boot Memory (EEPROM)
S/PDIF Optical Connectors
Codec ADAU1761
Figure 14: EVAL-AD2430WD1BZ board
EVAL-AD2430WC1BZ
The Figure 15 shows an EVAL-AD2430WC1BZ board which can be used as an A2B sub node. The board has following peripherals
AD2430 A2B transceiver
4 PDM Microphones
Figure 15: EVAL-AD2430WC1BZ board
EVAL-AD2428WB1BZ
Connections
To run the sample demo, the following setup connections are to be made.
Evaluation boards
A2B Evaluation boards shall be connected in the following order
EVAL-AD2430WD1BZ (Main) <–>EVAL-AD2428WB1BZ (Sub 0) <–> EVAL-AD2430WC1BZ (Sub 1) as shown in Figure 16
Connect twisted-pair wire between the A2B connector on the Main board and the “A” connector on the Sub 0 board.
Connect twisted-pair wire between the “B” connector on the Sub 0 board and the A2B connector on the Sub 1 board.
Connect 12V power supply to the power connector (P7) on AD2430WD1BZ board.
This connection is recommended for running the sample demo using PC as host. Refer Section 5 for more details on using
ADSP-21569 as host processor.
Figure 16: A2B Eval board connections
USBi
Attach an USBi cable to the main board connector P6 as shown in Figure 16. Other end of the cable should be connected to the PC.
This connection is required to override the schematic for the main node SigmaDSP ADAU1452. The connection is also used to directly control A2B system when PC is used as the target processor.
Audio In/out
Connect separate audio sources (
e.g., output from an iPod) to ‘Audio Line- in’ on AD2428WB1BZ as shown in Figure 16
Connect separate audio sinks (
e.g., active speakers) to ‘Audio Line-out’ ports, shown in Figure 16, on AD2430WD1BZ and AD2428WB1BZ.
Sample Demo Setup
Using SigmaStudio+ the A2B system can be directly controlled from a connected computer without involving a microcontroller or a DSP. This mode is helpful for quick testing of the capabilities of AD24xx without the need for a microcontroller in the system.
Please refer Appendices A and B for information about navigating in SigmaStudio+ for A2B use-case. A block diagram of a 3 node A2B system with PC as Host is shown below.
Figure 17: Sample A2B demo configuration
For PC Software setup, refer section 2.1.1 and for Hardware Setup refer section 4.1.2.4 . To run the sample demo, refer section 4.1.3 .
SC59x EZ-Kit Mode
This section describes the steps to run the demo using EV-SC594-SOM with AD2430.
*Note:* Running this demo requires CrossCore Embedded Studio to be installed on the machine. For details, refer section 2.1.1
Setup
The hardware connections to be done are described below.
A2B Evaluation boards shall be connected in the following order
EV-SC594-SOM (Rev B) ↔ EV-SOMCRR-EZKIT (Rev A) <–>Eval-AD2430WD1BZ(Main) ↔ EVAL-AD2428WB1BZ (Sub 0) <–> EVAL-AD2430WC1BZ (Sub 1) as shown in Figure 18
Connect twisted-pair wire between the “B” connector on the Main board and the “A” connector on the Sub 0 board. Repeat the same connection between Sub 0 and Sub 1
Connect 12V power supply to the power connector (P8) on EV-SOMCRR-EZKIT board.
Connect 12V power supply to the power connector (P7) on Eval-AD2430WDZ board.
Attach
JTAG to P1 on EV-SC594-SOM board and other end of
JTAG to
USB port of PC.
Connect audio source (
e.g., output from an iPod) to ‘Audio Line- in’ ports, shown in Figure 18, AD2428WB1BZ boards.
Connect separate audio sinks (
e.g., active speakers) to ‘Audio Line-out’ ports, shown Figure 18, on EV-SOMCRR-EZKIT and AD2428WB1BZ boards.
Figure 18: SC594-AD2430 setup
Jumper settings for EV-SOMCRR-EZKIT
There are no additional jumper settings needed for the purpose of this demo. The jumper settings should be maintained as mentioned in the EV-SOMCRR-EZKIT manual default configuration.
Running target framework on EV-SOMCRR EZ-KIT
Ensure that the “Boot Mode” switch is set to 0 on the EV-SC594-SOM EZ-KIT board.
Connect the
JTAG (ICE 1000 or ICE 2000) and power on the board with the setup as shown in 3.4.4.1 .
Create Debug Session in CCES by clicking Run → Debug Configurations → Application with CrossCore Debugger → Sharc → SC594 → Emulator → ICE 1000 / 2000 → Finish
Select the SC59x dxe to be loaded and click Debug to start the session as shown below.
In the Debug Window, Run F5 to execute sample demo.
Figure 19: Debug Configuration – SC59x