Wiki

The most recent version of this page is a draft.DiffThis version (09 Dec 2022 10:28) was approved by Gireesha Nirvanaiah.

This is an old revision of the document!


Click here to return to the Hardware Setup page

AD242x standard power

Evaluation boards

The Evaluation boards used in the AD242x demos are explained in the following subsections.

EVAL-AD2428WD1BZ

Figure 20 shows an EVAL-AD2428WD1BZ board which can be used as either an A2B main or sub node. The board has following components

  • AD2428 A2B transceiver
  • ADAU1452 SigmaDSP Audio Processor
  • 512K Self-Boot Memory (EEPROM)
  • S/PDIF Optical Connectors
  • Codec ADAU1761

Figure 20: EVAL-AD2428WD1BZ board

Jumper Settings

EVAL-AD2428WD1BZ without 1452 DSP Bypass
Jumper Action/Pin no Comments
Used as main-node
JP1 (A2B power) Install -
JP2 Uninstall Install when phantom power or hybrid power support is required
JP3 Uninstall Install when phantom power or hybrid power support is required
JP4 (BOOT) Install Self-Boot option disabled
JP5 (BCLK) 3-4 ADAU1452_BCLK_OUT0 → AD2428_BCLK
JP6 (SYNC) 3-4 ADAU1452_LRCLK_OUT0 → AD2428_SYNC
JP7 (DRX0) 3-4 ADAU1452_SDATA_OUT0 → AD2428_DRX0
JP8 (DRX1) 2-3 ADAU1452_SDATA_OUT1 → AD2428_DRX1 If Secondary Rx data line DRX1 is desired. Uninstall if only primary data line DRX0 is required.
JP9 (DTX1) 3-4 AD2428_DTX1 → ADAU1452_SDATA_IN1 If Secondary Tx data line DTX1 is desired. Uninstall if only primary data line DTX0 is required.
JP10 (DTX0) 1-2 AD2428_DTX0 → ADAU1452_SDATA_IN0
JP11 (ADMP621 CLK) Uninstall -
JP12 (NTC) Install -
JP13 (A2B_REG) Uninstall -
JP14 (VOLTAGE) Uninstall Install/ Uninstall depending on VIN requirement.
Installed → VIN = 7V
Uninstalled → VIN = 8V
JP19 (1961 BCLK) 1-2 ADAU1761 MCLK from CLKOUT of ADAU1452
- - -
Used as sub-node
JP1 (A2B power) Install -
JP2 Uninstall Install when phantom power or hybrid power support is required
JP3 Uninstall Install when phantom power or hybrid power support is required
JP4 (BOOT) Install Self-Boot option disabled
JP5 (BCLK) 3-4-5 AD2428_BCLK → ADAU1452_BCLK_OUT0 & ADAU1452_BCLK_IN0 (Use a three-way wire connector – Figure 21)
JP6 (SYNC) JP5(3-4) & JP7(5) AD2428_SYNC → ADAU1452_LRCLK_OUT0 & ADAU1452_LRCLK_IN0
JP7 (DRX0) 3-4 ADAU1452_SDATA_OUT0 → AD2428_DRX0 JP7.5 should be connected to SYNC signals on JP6.3 & JP6.4 (Use a three-way wire connector – Figure 21)
JP8 (DRX1) 2-3 ADAU1452_SDATA_OUT1 → AD2428_DRX1 If Secondary Rx data line DRX1 is desired. Uninstall if only primary data line DRX0 is required.
JP9 (DTX1) 3-4 AD2428_DTX1 → ADAU1452_SDATA_IN1 If Secondary Tx data line DTX1 is desired. Uninstall if only primary data line DTX0 is required.
JP10 (DTX0) 1-2 AD2428_DTX0 → ADAU1452_SDATA_IN0
JP11 (ADMP621 CLK) Uninstall -
JP12 (NTC) Install -
JP13 (A2B_REG) Uninstall -
JP14 (VOLTAGE) Uninstall Install depending on VIN requirement.
Installed → VIN = 7V
Uninstalled → VIN = 8V
JP19 (1961 BCLK) 1-2 ADAU1761 MCLK from CLKOUT of ADAU1452

Figure 21: Three way jumper connection

EVAL-AD2428WD1BZ with 1452 Without Bypass

Jumper Action/Pin no Comments
Used as main-node
JP1 (A2B power) Install -
JP2 Uninstall Install when phantom power or hybrid power support is required
JP3 Uninstall
JP4 (BOOT) Install Self-Boot option disabled
JP5 (BCLK) 3-4 ADAU1452_BCLK_OUT0 → AD2428_BCLK
JP6 (SYNC) 3-4 ADAU1452_LRCLK_OUT0 → AD2428_SYNC
JP7 (DRX0) 3-4 ADAU1452_SDATA_OUT0 → AD2428_DRX0
JP8 (DRX1) 2-3 ADAU1452_SDATA_OUT1 → AD2428_DRX1 If Secondary Rx data line DRX1 is desired. Uninstall if only primary data line DRX0 is required.
JP9 (DTX1) 3-4 AD2428_DTX1 → ADAU1452_SDATA_IN1 If Secondary Tx data line DTX1 is desired. Uninstall if only primary data line DTX0 is required.
JP10 (DTX0) 1-2 AD2428_DTX0 → ADAU1452_SDATA_IN0
JP11 (ADMP621 CLK) Uninstall -
JP12 (NTC) Install -
JP13 (A2B_REG) Uninstall -
JP14 (VOLTAGE) Uninstall Install/ Uninstall depending on VIN requirement.
Installed → VIN = 7V
Uninstalled → VIN = 8V
JP19 (1961 BCLK) 1-2 ADAU1761 MCLK from CLKOUT of ADAU1452
- - -
Used as sub-node
JP1 (A2B power) Install -
JP2 Uninstall Install when phantom power or hybrid power support is required
JP3 Uninstall Install when phantom power or hybrid power support is required
JP4 (BOOT) Install Self-Boot option disabled
JP5 (BCLK) 1-3 AD2428_BCLK → ADAU1961_BCLK
JP6 (SYNC) 1-3 AD2428_SYNC → ADAU1961_LRCLK
JP7 (DRX0) 1-3 ADAU1961_ADC → AD2428_DRX0
JP8 (DRX1) Uninstall -
JP9 (DTX1) Uninstall -
JP10 (DTX0) 2-3 AD2428_DTX0 → ADAU1961_DAC
JP11 (ADMP621 CLK) Uninstall -
JP12 (NTC) install -
JP13 (A2B_REG) Uninstall -
JP14 (VOLTAGE) Uninstall Install/ Uninstall depending on VIN requirement.
Installed → VIN = 7V
Uninstalled → VIN = 8V
JP19 (1961 BCLK) 2-3 ADAU1761 MCLK from AD2428_BCLK

EVAL-AD2428WB1BZ

The Figure 22 shows an EVAL-AD2428WB1BZ board which can be used as an A2B sub node. The board has following peripherals

  • AD2428 A2B transceiver
  • SigmaDSP with codec (ADAU1761).
  • 2 PDM Microphones
  • Push Button
  • EEPROM

Figure 22: EVAL-AD2428WB1BZ board

EVAL-AD2428WC1BZ

The Figure 23 shows an EVAL-AD2428WC1BZ board which can be used as an A2B sub node. The board has following peripherals

  • AD2428 A2B transceiver
  • 4 PDM Microphones

Figure 23: EVAL-AD2428WC1BZ board

Connections

To run the sample demo, the following setup connections are to be made.

Bus power sub-nodes

Evaluation boards

A2B Evaluation boards shall be connected in the following order

  1. EVAL-AD2428WD1BZ (Main) <–>EVAL-AD2428WC1BZ (Sub 0) <–> EVAL-AD2428WB1BZ (Sub 1) as shown in Figure 24
  2. Connect twisted-pair wire between the “B” connector on the Main board and the “A” connector on the Sub 0 board.
  3. Connect twisted-pair wire between the “B” connector on the Sub 0 board and the “A” connector on the Sub 1 board.
  4. Connect 12V power supply to the power connector (P4) on AD2428WD1BZ board.
This connection is recommended for running the sample demo using PC as host. Refer Section 7 for more details on using BF27, ADSP-21489 or ADSP-SC584 as host processor.

Figure 24: A2B Eval board connections

USBi

  • Attach an USBi cable to the main board connector P1 as shown in Figure 24. Other end of the cable should be connected to the PC.
  • This connection is required to override the schematic for the main node SigmaDSP ADAU1452. The connection is also used to directly control A2B system when PC is used as the target processor (no SDP-B board connected).

Audio In/out

  • Connect separate audio sources (e.g., output from an iPod) to ‘Audio Line- in’ ports, shown in Figure 24, on AD2428WD1BZ and AD2428WB1BZ boards.
  • Connect separate audio sinks (e.g., active speakers) to ‘Audio Line-out’ ports, shown in Figure 24, on AD2428WD1BZ and AD2428WB1BZ boards.
Do not connect the audio source directly from PC toWB1BZ board as they can cause ground loop issues. If connected discovery will fail for WB1BZ and subsequent nodes.

Figure 25: Two local powered AD2428WD1BZ boards (One of the audio stream is shown here)

As per Figure 25 two local powered nodes can be connected to each other to form an A2B network. One of them is a main node and the other is a sub node. This figure represents one of the two audio stream configurations. Figure 26 and Figure 27 represent the audio configurations with and without bypassing the 1452 DSP respectively. Connect audio sources and sinks as per these two figures.

Figure 26: Audio routing without 1452 DSP bypass

Figure 27: Audio routing with 1452 DSP bypass

/srv/wiki.analog.com/data/pages/resources/tools-software/a2bv2/quickstartguide/hardware-setup/ad242x-standard-power.txt · Last modified: 09 Dec 2022 11:23 by Gireesha Nirvanaiah