Click here to return to the Hardware Setup page
A2B Bus Analyzer
The A2B Bus Analyzer device can be used along with the A2B Evaluation boards to run the A2B Bus Analyzer demos
Figure 42 : A2B Bus Analyzer
Connections
To run the sample demos, the following setup connections are to be made.
Standard Power Main Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
Ordered List ItemA2B Bus Analyzer (Main Node Emulator) <–>EVAL-AD2433WB1BZ (Sub 0) <–> A2B Bus Analyzer (Bus Monitor) <–> EVAL-A2433WB1BZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a Standard Power Main Node Emulator and Bus Monitor.
Standard Power Sub Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
EVAL-AD2433WA1BZ (Main) <–>A2B Bus Analyzer (Bus Monitor) <–>A2B Bus Analyzer (Sub 0 Emulation) <–> EVAL-AD2433WB1BZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a Standard Power Sub Node Emulator and Bus Monitor.
High Power Main Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
A2B Bus Analyzer (High Power Main Node Emulator) <–>EVAL-AD2435WJ3LZ (Sub 0) <–> A2B Bus Analyzer (Bus Monitor) <–> EVAL-AD2435WJ3LZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a High-Power Main Node Emulator and Bus Monitor
High Power Sub Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
EVAL-AD2435WA3LZ (Main) <–>A2B Bus Analyzer (Sub 0 Emulation) <–> A2B Bus Analyzer (Bus Monitor) <–>EVAL-AD2435WJ3LZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a High-Power Sub Node Emulator and Bus Monitor.
242x Main Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
A2B Bus Analyzer (242x Main Node Emulator) <–>EVAL-AD2428WC1BZ (Sub 0) <–> A2B Bus Analyzer (Bus Monitor) <–> EVAL-AD2428WB1BZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a 242x Main Node Emulator and Bus Monitor
242x Sub Node Emulation and Bus Monitor
A2B Bus Analyzer device and A2B Evaluation boards shall be connected in the following order
EVAL-AD2428WD1Z (Main) <–>A2B Bus Analyzer (Bus Monitor) <–> A2B Bus Analyzer (Sub 0 Emulation) <–>EVAL-AD2428WB1BZ (Sub 1)
Refer the
A2B Bus Analyzer QSG for setting up the A2B Bus Analyzer as a 242x Sub Node Emulator and Bus Monitor.