Click here to return to the QSG homepage
APPENDIX I: Plugin Upgrades
Plugins can be upgraded to a higher version (if it exists) using either of the following methods
Plugin upgrades
Project version control
On the toolbar click on Tools → project version control. A version control tab will open up.
Select plugin version management.
A list of plugins will be listed in this window as shown in
Figure 109.
Select an available plugin version and click on “upgrade”.
Figure 109: Plugin version upgrade through version control
Upgrade of AnalogDevices.Plugins.Channels.A2BChannel is not supported.
Properties window
Single left-click any plugin on the canvas
As shown in
Figure 110, on the properties window towards the right, select the required version from the drop-down next to Version.
Figure 110: Plugin version upgrade through Properties window