Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:a2bv2:quickstartguide:appendix-e [25 Nov 2022 07:40] – [Context Menu’s on Rx Crossbar] Gireesha Nirvanaiahresources:tools-software:a2bv2:quickstartguide:appendix-e [08 Dec 2022 13:00] (current) – [Crossbar View] Gireesha Nirvanaiah
Line 1: Line 1:
 +[[:resources:tools-software:a2bv2:quickstartguide|Click here to return to the QSG homepage]]
 +
 ====== APPENDIX E: Crossbar View & Configuration ====== ====== APPENDIX E: Crossbar View & Configuration ======
 Crossbar view is available for all the nodes. Crossbar view is available for all the nodes.
Line 11: Line 13:
 In addition to the above, Crossbar view for main node supports offset on the TX pins which can be configured using the register (A2B_I2STXOFFSET.TXOFFSET). In addition to the above, Crossbar view for main node supports offset on the TX pins which can be configured using the register (A2B_I2STXOFFSET.TXOFFSET).
  
-**Hint:** Tx Offset adjustment is not supported for sub-nodes, only supported on main node+**Hint :** Tx Offset adjustment is not supported for sub-nodes, only supported on main node
  
 ===== Crossbar View Dependencies Configuration ===== ===== Crossbar View Dependencies Configuration =====
 ==== Number of Tx/Rx Pins Configuration ==== ==== Number of Tx/Rx Pins Configuration ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:number_of_tx_rx_pins_configuration.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:number_of_tx_rx_pins_configuration.png?300|}} 
 + 
 +**Figure 86 :** Number of Tx/Rx Pins Configuration
 ==== TX Crossbar registers (A2B_TXXBAR0 - A2B_TXXBAR31) ==== ==== TX Crossbar registers (A2B_TXXBAR0 - A2B_TXXBAR31) ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:tx_crossbar_registers_a2b_txxbar0_-_a2b_txxbar31_.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:tx_crossbar_registers_a2b_txxbar0_-_a2b_txxbar31_.png?300|}} 
 + 
 +**Figure 87 :** TX Crossbar registers (A2B_TXXBAR0 - A2B_TXXBAR31)
 ==== RX Crossbar registers (A2B_RXMASK0 - A2B_RXMASK7) ==== ==== RX Crossbar registers (A2B_RXMASK0 - A2B_RXMASK7) ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:rx_crossbar_registers_a2b_rxmask0_-_a2b_rxmask7_.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:rx_crossbar_registers_a2b_rxmask0_-_a2b_rxmask7_.png?300|}} 
 + 
 +**Figure 88 :** RX Crossbar registers (A2B_RXMASK0 - A2B_RXMASK7)
 ==== TDM Mode & Tx/Rx Interleave Configuration ==== ==== TDM Mode & Tx/Rx Interleave Configuration ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:tdm_mode_tx_rx_interleave_configuration.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:tdm_mode_tx_rx_interleave_configuration.png?300|}}
  
 +**Figure 89 :** TDM Mode & Tx/Rx Interleave Configuration
 ===== Crossbar View ===== ===== Crossbar View =====
-For example, considering the 3-node schematic with the stream configuration example, crossbar view looks like as mentioned in the snapshots for all the nodes+For example, considering the 3-node schematic with the [[:resources:tools-software:a2bv2:quickstartguide:appendix-e#crossbar_view|stream configuration example]], crossbar view looks like as mentioned in the snapshots for all the nodes
  
 ==== Sample Stream Definition & Assignment for 3 node schematics ==== ==== Sample Stream Definition & Assignment for 3 node schematics ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:sample_stream_definition_assignment_for_crossbar_view_visualization.png?400 |}}+{{:resources:tools-software:a2bv2:quickstartguide:sample_stream_definition_assignment_for_crossbar_view_visualization.png?400|}} 
 + 
 +**Figure 90 :** Sample Stream Definition & Assignment for Crossbar view visualization
 ==== Crossbar view at Main node with no Tx offset ==== ==== Crossbar view at Main node with no Tx offset ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node.png?400 |}}+{{:resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node.png?400|}} 
 + 
 +**Figure 91 :** Crossbar view at Main node
 ==== Crossbar view at sub node – 0 ==== ==== Crossbar view at sub node – 0 ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_sub_node_0.png?400 |}}+{{:resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_sub_node_0.png?400|}} 
 + 
 +**Figure 92 :** Crossbar view at sub node – 0 
 + 
 +<note>The channel D0 and D1 received on RX0 pin is “MicIn” stream. Because of the data-tunnel addition, the stream colour is mis-represented in RX0. This is under investigation and will be updated in next release.</note>
 ==== Crossbar view at sub node – 1 ==== ==== Crossbar view at sub node – 1 ====
  
-{{ :resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_sub_node_1.png?400 |}}+{{:resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_sub_node_1.png?400|}} 
 + 
 +**Figure 93 :** Crossbar view at sub node – 1
 ==== Crossbar view at Main node with Tx Offset ==== ==== Crossbar view at Main node with Tx Offset ====
-{{ :resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node_with_tx_offset.png?300 |}}+The below snapshot is taken with the Tx Offset value “4” on TX 0 pin 
 + 
 +{{:resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node_with_tx_offset.png?300|}} 
 + 
 +**Figure 94 :** Crossbar view at Main node with Tx Offset
 ==== Crossbar view at Main node with Tx Interleave enabled ==== ==== Crossbar view at Main node with Tx Interleave enabled ====
 The similar way Rx Interleave also works. The similar way Rx Interleave also works.
  
-{{ :resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node_with_tx_rx_interleave_enabled.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:crossbar_view_at_main_node_with_tx_rx_interleave_enabled.png?300|}} 
 + 
 +**Figure 95 :** Crossbar view at Main node with Tx & Rx Interleave enabled
  
  
Line 57: Line 82:
   * Reset Channel Map (this option reset’s channel mapping if any mapping is done manually on crossbar)   * Reset Channel Map (this option reset’s channel mapping if any mapping is done manually on crossbar)
  
-{{ :resources:tools-software:a2bv2:quickstartguide:context_menu_s_on_tx_pin_of_crossbar_at_main_node.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:context_menu_s_on_tx_pin_of_crossbar_at_main_node.png?300|}} 
 + 
 +**Figure 96 :** Context Menu's on Tx Pin of Crossbar at Main Node
 ==== Context Menu’s on Rx Crossbar ==== ==== Context Menu’s on Rx Crossbar ====
 Crossbar supports the below options on Rx pin as shown in the below snapshot: Crossbar supports the below options on Rx pin as shown in the below snapshot:
Line 63: Line 90:
   * Clear Mapping (this option clears the mapping of a particular slot on the Rx pin)   * Clear Mapping (this option clears the mapping of a particular slot on the Rx pin)
  
-{{ :resources:tools-software:a2bv2:quickstartguide:context_menu_s_on_rx_crossbar.png?300 |}}+{{:resources:tools-software:a2bv2:quickstartguide:context_menu_s_on_rx_crossbar.png?300|}} 
 + 
 +**Figure 97 :** Context Menu's on Rx Crossbar
  
  
  
resources/tools-software/a2bv2/quickstartguide/appendix-e.txt · Last modified: 08 Dec 2022 13:00 by Gireesha Nirvanaiah