Click here to return to the QSG homepage
APPENDIX D: Building ADSP-2156x Project
To build the ADSP-2156x project from the SS Plus installer path: “C:\Analog Devices\SigmaStudioPlus-Rel1.2.0\Target\Examples\Demo\ADSP-2156x\ADSP-21569\SS_App_Core1”, following steps need to be followed.
Import the project into CCES
Open “Properties” by right clicking on the project and navigate to “C/C++ Build → Settings”
Remove the macro “ADSP_21569_SOM” from the CrossCore Sharc C/C++ Compiler/Preprocessor Menu as shown in Figure 82.
Figure 82: Removal of Macro
To provide BCLK and Frame Sync to A2B transceiver, navigate to “system.svc” in the project and open “Signal Routing Unit”.
Under “DAI0 Pin Buffer” following changes need to be made.
Figure 83: DAI0_PB03_I Configuration
Figure 84: DAI0_PB04_I Configuration
In the file “C:\Analog Devices\CrossCore Embedded Studio 2.10.0\SHARC\include\drivers\sport\ adi_sport_2156x.h”, the value of
ADI_SPORT_BLOCKING_MODE must be set to “1u” as shown in Figure 85.
Figure 85: SPORT Blocking Mode Macro Value Update