Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:a2bv2:quickstartguide:appendix-b [08 Dec 2022 13:48] – [Navigating to Stream and Export Configuration in SS+] Gireesha Nirvanaiahresources:tools-software:a2bv2:quickstartguide:appendix-b [19 Oct 2023 12:04] (current) – [Command List Utility] Gireesha Nirvanaiah
Line 63: Line 63:
 Export settings window as shown in [[:resources:tools-software:a2bv2:quickstartguide:appendix-b#export_configuration|Figure 68]] provides options to export BusConfig.c, Commandlist.h and Commandlist.xml files which can be used in Target Mode. Export settings window as shown in [[:resources:tools-software:a2bv2:quickstartguide:appendix-b#export_configuration|Figure 68]] provides options to export BusConfig.c, Commandlist.h and Commandlist.xml files which can be used in Target Mode.
  
-{{:resources:tools-software:a2bv2:quickstartguide:export_settings.png?500|}}+{{:resources:tools-software:a2bv2:quickstartguide:export-import.png?600|}}
  
 **Figure 68 :** Export Settings **Figure 68 :** Export Settings
Line 105: Line 105:
 Multi-main export configuration will export a single BCF xml and/or c file for the current multi-main network. This is feature is applicable only for multi-main networks. Multi-main export configuration will export a single BCF xml and/or c file for the current multi-main network. This is feature is applicable only for multi-main networks.
  
 +
 +==== Command List Utility ====
 +Command list utility allows user to merge primary and secondary branch command list into a single command list to support branching. 
 +
 +{{:resources:tools-software:a2bv2:quickstartguide:command_list_merge.png?600|}}
 +
 +**Figure:** Command List Merge
 +
 +  - Generate the command list file from primary branch A2B network schematic. 
 +  - Generate the command list file from secondary branch A2B network schematic.
 +  - Use the command list merge utility feature to generate the merged command list from primary branch and secondary branch command list files.
 +  - Click on the CmdLstMerge Tab as indicated above in Figure.
 +  - Select primary branch command list file generated in step 1 in “File path for Primary Branch .XML file”
 +  - Select secondary branch command list file generated in step 2 in “File path for Secondary Branch .XML file” 
 +  - Provide the file path location for merged command list file in “File path for Merged Branching .XML file”
 +  - In the “Primary Branch Sub-Node ID” field, enter the sub-node id to which the secondary branch is connected in the primary chain.
 +  - Select the secondary branch main node address from “Chip Address” drop down box.
 +  - Click on the Export button to generate merged command list.
 +  - Use the Sequence window to Discover and configure the Branching network with generated merged command list file.
resources/tools-software/a2bv2/quickstartguide/appendix-b.txt · Last modified: 19 Oct 2023 12:04 by Gireesha Nirvanaiah