This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:a2bv2:quickstartguide:appendix-b [19 Oct 2023 11:58] – [Command List Utility] Gireesha Nirvanaiah | resources:tools-software:a2bv2:quickstartguide:appendix-b [19 Oct 2023 12:04] (current) – [Command List Utility] Gireesha Nirvanaiah | ||
---|---|---|---|
Line 110: | Line 110: | ||
{{: | {{: | ||
+ | |||
+ | **Figure:** Command List Merge | ||
+ | |||
+ | - Generate the command list file from primary branch A2B network schematic. | ||
+ | - Generate the command list file from secondary branch A2B network schematic. | ||
+ | - Use the command list merge utility feature to generate the merged command list from primary branch and secondary branch command list files. | ||
+ | - Click on the CmdLstMerge Tab as indicated above in Figure. | ||
+ | - Select primary branch command list file generated in step 1 in “File path for Primary Branch .XML file” | ||
+ | - Select secondary branch command list file generated in step 2 in “File path for Secondary Branch .XML file” | ||
+ | - Provide the file path location for merged command list file in “File path for Merged Branching .XML file” | ||
+ | - In the “Primary Branch Sub-Node ID” field, enter the sub-node id to which the secondary branch is connected in the primary chain. | ||
+ | - Select the secondary branch main node address from “Chip Address” drop down box. | ||
+ | - Click on the Export button to generate merged command list. | ||
+ | - Use the Sequence window to Discover and configure the Branching network with generated merged command list file. |