Wiki

This version (09 Oct 2023 14:34) was approved by Praveen Kumar.

Click here to return to the A2B SSPLUS User Guide homepage

Network Analysis and Debug

SigmaStudioPlus allows user to estimate important network parameters like Bandwidth and power consumption. It also allows user to monitor real-time bit errors in the system using pseudo or actual bit stream. This option can be accessed using the Right-Click menu of the Main Transceiver node as shown in below figure. Note that calculate… option is accessible only if the A2B schematic is ‘Link’ed after the last schematic modification. Save schematic and click on the ‘Link’ icon if the option is disabled.

Figure : Calculation Option

For additional information on Bandwidth Calculation, Power Calculation, BERT, and Debug, refer Network Analysis and Debug section in QSG.

resources/tools-software/a2bv2/a2bssplususerguide/networkanalysisanddebug.txt · Last modified: 06 Oct 2023 11:28 by Gireesha Nirvanaiah