Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:a2b-bus-analyzer:sdk-user-guide [12 Aug 2022 13:50] – Better paths for examples S Fernandezresources:tools-software:a2b-bus-analyzer:sdk-user-guide [15 Nov 2022 13:53] (current) – Updated to python 3.8 S Fernandez
Line 72: Line 72:
  
 **Note**: While there is a copy of the binaries in the "Release" folder, since the shared libraries are not in the path, the example will fail to run. **Note**: While there is a copy of the binaries in the "Release" folder, since the shared libraries are not in the path, the example will fail to run.
- 
-To run the application, change directory into the 'Release' folder and enter the executable's name: 
  
 <code> <code>
Line 107: Line 105:
  
 ^ ^**Platform** ^**Details** ^ ^ ^**Platform** ^**Details** ^
-|{{:resources:tools-software:a2b-bus-analyzer:image2.png?20|}}|Windows | a2ba_sdk-3.0.0-cp36-cp36m-win_amd64.whl | +|{{:resources:tools-software:a2b-bus-analyzer:image2.png?20|}}|Windows | a2ba_sdk-3.0.0-cp38-cp38m-win_amd64.whl | 
-|{{:resources:tools-software:a2b-bus-analyzer:image3.png?20|}}|Linux   | a2ba_sdk-3.0.0-cp36-cp36m-linux_x86_64.whl      | +|{{:resources:tools-software:a2b-bus-analyzer:image3.png?20|}}|Linux   | a2ba_sdk-3.0.0-cp38-cp38m-linux_x86_64.whl      | 
-|{{:resources:tools-software:a2b-bus-analyzer:image4.png?20|}}|macOS   | a2ba_sdk-3.0.0-cp36-cp36m-macosx_10_15_x86_64.whl                     |+|{{:resources:tools-software:a2b-bus-analyzer:image4.png?20|}}|macOS   | a2ba_sdk-3.0.0-cp38-cp38m-macosx_10_15_x86_64.whl                     |
  
-**Note:** Currently the SDK supports only Python 3.6. **Python 2 is not supported**.+**Note:** Currently the SDK supports only Python 3.8. **Python 2 is not supported**.
  
 ==== Installation ==== ==== Installation ====
Line 131: Line 129:
  
 # Install SDK wheel to new virtual environment # Install SDK wheel to new virtual environment
-(env) > pip install a2ba_sdk-3.0.0-cp36-cp36m-win_amd64.whl  # WINDOWS - choose correct wheel for your platform+(env) > pip install a2ba_sdk-3.0.0-cp38-cp38m-win_amd64.whl  # WINDOWS - choose correct wheel for your platform
  
 </code> </code>
resources/tools-software/a2b-bus-analyzer/sdk-user-guide.txt · Last modified: 15 Nov 2022 13:53 by S Fernandez