Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:technical-guides:motif:simulink [19 Mar 2015 18:20] – [Install MOTIF] Di Puresources:technical-guides:motif:simulink [31 Dec 2020 06:14] (current) – fix links Robin Getz
Line 32: Line 32:
 ====== AD9625 Example ====== ====== AD9625 Example ======
  
-AD9625 is a 12-Bit, 2.5 GSPS/2.0 GSPS, 1.3 V/2.5 V Analog-to-Digital Converter. Its data sheet can be found [[http://www.analog.com/media/en/technical-documentation/data-sheets/AD9625.pdf|here]].+AD9625 is a 12-Bit, 2.5 GSPS/2.0 GSPS, 1.3 V/2.5 V Analog-to-Digital Converter. Its data sheet can be found [[adi>AD9625|here]].
  
 To use the AD9625 model, go to \AD9625\MOTIF directory, and double click on <file>Main.m</file> to open the main function. To use the AD9625 model, go to \AD9625\MOTIF directory, and double click on <file>Main.m</file> to open the main function.
resources/technical-guides/motif/simulink.txt · Last modified: 31 Dec 2020 06:14 by Robin Getz