This is an old revision of the document!
This document intention is to provide some tips and basic considerations when using ADI ADXL accelerometers. We thank you for choosing ADI and want to let you know that our main focus is to offer High Performance Inertial Sensors for the most demanding applications.
The first and most important advise we would like to offer when using our ADXL portfolio is to carefully read the product datasheet, this can save you precious time.
The FSR is the guaranteed dynamic range at the output of the signal chain. FSR is specified as a minimum value and is guaranteed across all conditions. Acceleration measurement may be possible beyond this minimum value. However, performance characteristics are not guaranteed.
Device nonlinearity is the maximum deviation of any sensor data point from the least squares linear fit of the acceleration data set at an equivalent input acceleration level. The acceleration data set can encompass any range of applied acceleration, up to the complete FSR. Nonlinearity is defined mathematically as
where: ACCMEAS is the measured acceleration at a defined gn. ACCFIT is the predicted acceleration at a defined gn. gn is the input acceleration level.
Cross axis sensitivity is the measured output of the device in response to input stimuli orthogonal to the intended sense axis. It is measured as a percentage of the applied acceleration, as follows:
where: ACCMEAS(gx) is the measured x-axis acceleration. gy is the applied y-axis acceleration. gz is the applied z-axis acceleration.
The cross axis sensitivity specification accounts for device level cross axis components only. These components include variations in sensor fabrication and the alignment of the sensor to the orthogonal axes of the package (also known as package alignment error). The cross axis specification does not account for system level sources of misalignment (for example, on the PCB or module).
fo is the natural frequency at which the MEMS element has a higher gain when subjected to acceleration events. Input acceleration at this resonant frequency causes the sensor to displace by an amount equal to the applied acceleration multiplied by the quality factor (Q). Some parts use different sensor types for the horizontal (x- and y-axes) and the vertical (z-axis) sensing axes. Therefore, the resonant frequency responses of these sensors are not the same.
The quality factor is a scalar factor that governs the increase or decrease in amplitude of an acceleration signal applied at the resonant frequency of a MEMS element.
Sensitivity is the slope of the line of best fit for the acceleration transfer function, as measured across the output FSR. The sensitivity defines the change in output (LSB) per unit change of input (g). The inverse, scale factor, is in units of g/LSB.
Measurement resolution specifies the number of data bits in each acceleration data-word. For example, the 14-bit measurement of the ADXL317 has 16,384 bits of resolution. For an FSR of ±16 g (32 g total), this resolution yields a sensitivity of 500 LSB/g and a scale factor of 2.0 mg/LSB.
The zero g bias error (also called offset) is any static error term on the sensor output. Zero g bias error is measured as the deviation from 0 g with no externally applied acceleration (including gravity). To more accurately measure offset, take measurements at orientations of +1 g and –1 g and average the results. Each measurement must be taken over a sufficiently long time window to reduce the influence of external physical stimuli that may exist in the measurement system.
Initial zero g output deviation is the error level at ambient conditions, measured immediately after completion of device manufacture. The initial zero g output deviation value denotes the standard deviation of the measured offset values across a large population of devices.
For applied ac acceleration, the cutoff (−3 dB) frequency is the frequency at which the input stimulus is attenuated in amplitude by 29.3% (1 − √2/2) at the output of the signal chain.
It is important to respect the power supply limits and considerations described in the datasheet.
Some products, e.g. ADXL313, specifies that VS and VDDIO can be applied in any sequence without damaging the part, whereas the the ADXL355 specifies that, VS cannot be powered before VDDIO.
Generally it is recommend to use a 0.1uF ceramic capacitor and a 1-to-10uF tantalum capacitor between VS/VDDIO. Following this recommendation is very important to meet the datasheet specifications, for example in terms of noise level.
It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always start up the accelerometer from ground level (0 V) to ensure proper operation. If this is not possible, care must be taken regarding the following specifications:
To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/output (GPIO), connect a shutdown discharge switch to the supply, or use a voltage regulator with a shutdown discharge feature.