This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:technical-guides:best_engineering_practices_when_using_adxl_accelerometers [29 Mar 2021 19:16] – Pablo del Corro | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Best Engineering practices when using ADXL accelerometers ====== | ||
+ | ===== Introduction ===== | ||
+ | This document intention is to provide some tips and basic considerations when using ADI ADXL accelerometers. | ||
+ | We thank you for choosing ADI and want to let you know that our main focus is to offer High Performance Inertial Sensors for the most demanding applications. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The first and most important advise we would like to offer when using our ADXL portfolio is to **carefully read the product datasheet**, | ||
+ | |||
+ | ===== Terminology ===== | ||
+ | |||
+ | === Full-Scale Range (FSR) === | ||
+ | The FSR is the guaranteed dynamic range at the output of the signal chain. FSR is specified as a minimum value and is guaranteed across all conditions. Acceleration measurement may be possible beyond this minimum value. However, performance characteristics are not guaranteed. | ||
+ | |||
+ | === Nonlinearity === | ||
+ | Device nonlinearity is the maximum deviation of any sensor data point from the least squares linear fit of the acceleration data set at an equivalent input acceleration level. The acceleration data set can encompass any range of applied acceleration, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | where: | ||
+ | ACCMEAS is the measured acceleration at a defined gn. | ||
+ | ACCFIT is the predicted acceleration at a defined gn. | ||
+ | gn is the input acceleration level. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | === Cross Axis Sensitivity === | ||
+ | Cross axis sensitivity is the measured output of the device in response to input stimuli orthogonal to the intended sense axis. It is measured as a percentage of the applied acceleration, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | where: | ||
+ | ACCMEAS(gx) is the measured x-axis acceleration. | ||
+ | gy is the applied y-axis acceleration. | ||
+ | gz is the applied z-axis acceleration. | ||
+ | |||
+ | The cross axis sensitivity specification accounts for device level cross axis components only. These components include variations in sensor fabrication and the alignment of the sensor to the orthogonal axes of the package (also known as package alignment error). The cross axis specification does not account for system level sources of misalignment (for example, on the PCB or module). | ||
+ | |||
+ | === Resonant Frequency (fo) === | ||
+ | fo is the natural frequency at which the MEMS element has a higher gain when subjected to acceleration events. Input acceleration at this resonant frequency causes the sensor to displace by an amount equal to the applied acceleration multiplied by the quality factor (Q). | ||
+ | Some parts use different sensor types for the horizontal (x- and y-axes) and the vertical (z-axis) sensing axes. Therefore, the resonant frequency responses of these sensors are not the same. | ||
+ | |||
+ | === Quality Factor === | ||
+ | The quality factor is a scalar factor that governs the increase or decrease in amplitude of an acceleration signal applied at the resonant frequency of a MEMS element. | ||
+ | |||
+ | === Sensitivity === | ||
+ | Sensitivity is the slope of the line of best fit for the acceleration transfer function, as measured across the output FSR. The sensitivity defines the change in output (LSB) per unit change of input (g). The inverse, scale factor, is in units of g/LSB. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | === Measurement Resolution === | ||
+ | Measurement resolution specifies the number of data bits in each acceleration data-word. For example, the 14-bit measurement of the ADXL317 has 16,384 bits of resolution. For an FSR of ±16 g (32 g total), this resolution yields a sensitivity of 500 LSB/g and a scale factor of 2.0 mg/LSB. | ||
+ | |||
+ | === Zero g Bias Error === | ||
+ | The zero g bias error (also called offset) is any static error term on the sensor output. Zero g bias error is measured as the deviation from 0 g with no externally applied acceleration (including gravity). | ||
+ | To more accurately measure offset, take measurements at orientations of +1 g and –1 g and average the results. Each measurement must be taken over a sufficiently long time window to reduce the influence of external physical stimuli | ||
+ | that may exist in the measurement system. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | === Initial Zero g Output Deviation === | ||
+ | Initial zero g output deviation is the error level at ambient conditions, measured immediately after completion of device manufacture. The initial zero g output deviation value denotes the standard deviation of the measured offset values across a large population of devices. | ||
+ | |||
+ | === Cutoff (−3 dB) Frequency === | ||
+ | For applied ac acceleration, | ||
+ | to the low-pass cascaded integrated comb (CIC) filter and the low-pass infinite impulse response (IIR) filter setting as selected by the user. A high-pass filter can also be turned on by the user but is disabled by default. All other signal chain elements have an appreciably high bandwidth and are not significant contributors to the cutoff frequency. | ||
+ | |||
+ | === Noise Density === | ||
+ | Noise density is a measure of the inherent noise and is a combination of all internal noise sources. This density is fixed by the architecture of the device and is independent of bandwidth. See the Filtering: Noise and Latency Considerations section for more information on noise density. | ||
+ | Output Noise | ||
+ | Output noise is the realized noise in reported measurements. Whereas noise density expresses the inherent noise in the device, output noise is the union of density and bandwidth. Filters with lower bandwidths provide more aggressive filtering and, therefore, greater noise reduction than filters with higher bandwidths. | ||
+ | |||
+ | ===== Power supply considerations ===== | ||
+ | It is important to respect the power supply limits and considerations described in the datasheet. | ||
+ | |||
+ | <note tip>As a general rule, it is __highly recommended__ to always be started up the accelerometer from ground level (0 V).</ | ||
+ | |||
+ | === Recommended VS and VDDIO power sequencing === | ||
+ | Some products, e.g. ADXL313, specifies that VS and VDDIO can be applied in any sequence without damaging the part, whereas the the ADXL355 specifies that, VS cannot be powered before VDDIO. | ||
+ | | ||
+ | === Power supply decoupling specifications === | ||
+ | Generally it is recommend to use a 0.1uF ceramic capacitor and a 1-to-10uF tantalum capacitor between VS/VDDIO. Following this recommendation is very important to meet the datasheet specifications, | ||
+ | |||
+ | === Power Cycling === | ||
+ | It is common in ULP applications to power cycle the accelerometer to reduce power consumption. When using this technique, please remember that it is highly recommend to always start up the accelerometer from ground level (0 V) to ensure proper operation. | ||
+ | If this is not possible, care must be taken regarding the following specifications: | ||
+ | |||
+ | * __**VS supply start-up threshold**__: | ||
+ | * __**Hold time**__: VS and VDDIO supplies must be held below 100 mV for at least 200 ms before re-powering the part. | ||
+ | * __**Rise time**__: For the worst case scenario (100mV Vs starts up and 200ms hold time) VS and VDDIO supplies rise time must be linear and within 250 μs to reach the supply lower range voltage. For example, for the ADXL372, the power supply lower range voltage is 1.6V, thus the voltage supply should raise from 0V to 1.6V within 250μs. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | < | ||
+ | | ||
+ | To enable supply discharge, it is recommended to power the device from a microcontroller general-purpose input/ | ||
+ | |||
+ | |||
+ |