This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:quick-start:ad5760 [15 Apr 2013 15:38] – remove part numbers in several places Yuet Ng | resources:quick-start:ad5760 [22 Apr 2013 21:11] (current) – add C[2:0] to table 6 Yuet Ng | ||
---|---|---|---|
Line 16: | Line 16: | ||
* 35 MHz Schmitt triggered digital interface | * 35 MHz Schmitt triggered digital interface | ||
* 1.8 V compatible digital interface | * 1.8 V compatible digital interface | ||
- | \\ | ||
===== Functional Block Diagram===== | ===== Functional Block Diagram===== | ||
{{ : | {{ : | ||
Line 22: | Line 21: | ||
<WRAP clear></ | <WRAP clear></ | ||
- | \\ | ||
===== Pin Configuration ===== | ===== Pin Configuration ===== | ||
\\ | \\ | ||
Line 179: | Line 177: | ||
* Keep the default mode for SDODIS and RBUF. | * Keep the default mode for SDODIS and RBUF. | ||
* To write in binary coding, select BIN/2sC = 1. | * To write in binary coding, select BIN/2sC = 1. | ||
- | * Set DACTRI = 0 and OPGND = 0 to remove the DAC output clamp to ground and place the DAC in normal operating mode. | + | * Set DACTRI = 0 and OPGND = 0 to place the DAC in normal operating mode and remove the DAC output clamp to ground, respectively. |
Write the following over the serial interface: 0010 0000 0000 0000 0001 0010 (R/< | Write the following over the serial interface: 0010 0000 0000 0000 0001 0010 (R/< | ||
Line 190: | Line 188: | ||
^Bit(s) | ^Bit(s) | ||
|23 |R/< | |23 |R/< | ||
+ | |[22: | ||
|5 |SDODIS | |5 |SDODIS | ||
|4 |BIN/ | |4 |BIN/ | ||
- | |[3:2] | + | |3 |DACTRI |
+ | |2 |OPGND |0 | Remove the DAC output clamp to ground | | ||
|1 |RBUF | 1 |The internal amplifier powered down | | |1 |RBUF | 1 |The internal amplifier powered down | | ||
Line 215: | Line 215: | ||
* Set D[19:0], the data bits, for a midscale code. | * Set D[19:0], the data bits, for a midscale code. | ||
- | The 24-bit data to write over the serial interface is: | + | The 24-bit data to write over the serial interface is as follows: |
\\ | \\ | ||
\\ | \\ | ||
Line 269: | Line 269: | ||
\\ | \\ | ||
{{ : | {{ : | ||
- | <WRAP CENTERALIGN>// | + | <WRAP CENTERALIGN>// |
\\ | \\ | ||
\\ | \\ | ||
Line 305: | Line 305: | ||
See Figure 10. | See Figure 10. | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Note that this action is a read function. Therefore, set the R/< | + | Note that this action is a read function. Therefore, set the R/< |
\\ | \\ | ||
\\ | \\ |