Single, 16-/18-/20-Bit, Voltage Output DACs, SPI Interface
Figure 2. 24-Lead LFCSP Pin Configuration
Table 1. Function Descriptions for Quick Start
Mnemonic | Description |
---|---|
VOUT | Analog output voltage. |
VREFP | Positive reference voltage input. Connect a voltage in the range of 5 V to VDD - 2.5 V. |
VDD | Positive analog supply connection. Connect a voltage in the range of 7.5 V to 16.5 V. VDD must be decoupled to AGND. |
Active low reset. Asserting this pin returns the DAC to its power-on status. | |
Active low input. Asserting this pin sets the DAC register to a user defined value and updates the DAC output. | |
Active low load DAC logic input. This is used to update the DAC register and, consequently, the analog output. | |
VCC | Digital supply. Connect a voltage in the range of 2.7 V to 5.5 V. VCC must be decoupled to DGND. |
IOVCC | Digital interface supply. Voltage range is from 1.71 V to 5.5 V. |
SDO | Serial data output. |
SDIN | Serial data input. |
SCLK | Serial clock input. |
Level triggered control input (active low). This is the frame synchronization signal for the input data. | |
DGND | Ground reference for digital circuitry. |
VREFN | Negative reference voltage input. Connect a voltage in the range of VSS + 2.5 V to 0 V. |
VSS | Negative analog supply connection. Connect a voltage in the range of -16.5 V to -2.5 V. VSS must be decoupled to AGND. |
AGND | Ground reference for analog circuitry. |
RFB | Feedback connection for external amplifier. |
INV | Inverting input connection for external amplifier. |
Table 2. Hardware Control Pins Truth Table
/LDAC | /CLR | /RESET | Function |
---|---|---|---|
X1 | X1 | 0 | DAC in reset mode. The device cannot be programmed. |
X1 | X1 | ⇑2 | DAC is returned to its power-on state. All registers are set to their default values. |
0 | 0 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
0 | 1 | 1 | Output set according to the DAC register value. |
1 | 0 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
⇓3 | 1 | 1 | Output set according to the DAC register value. |
⇓3 | 0 | 1 | Output remains at the clearcode register value. |
⇑2 | 1 | 1 | Output remains set according to the DAC register value. |
⇑2 | 0 | 1 | Output remains at the clearcode register value. |
1 | ⇓3 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
0 | ⇓3 | 1 | DAC register loaded with the clearcode register value and output set accordingly. |
1 | ⇑2 | 1 | Output remains at the clearcode register value. |
0 | ⇑2 | 1 | Output set according to the DAC register value. |
1 X is don't care.
2 ⇑ is rising edge.
3 ⇓ is falling edge.
Figure 3. Input Shift Register Contents
Table 3. Register Address Definitions
Register Address | ||||
---|---|---|---|---|
Read/Write (R/W) | C2 | C1 | C0 | Description |
X1 | 0 | 0 | 0 | No operation |
0 | 0 | 0 | 1 | Write to the DAC register |
0 | 0 | 1 | 0 | Write to the control register |
0 | 0 | 1 | 1 | Write to the clearcode register |
0 | 1 | 0 | 0 | Write to the software control register |
1 | 0 | 0 | 1 | Read from the DAC register |
1 | 0 | 1 | 0 | Read from the control register |
1 | 0 | 1 | 1 | Read from the clearcode register |
1 X = don't care.
Figure 4. Control Register
Table 4. Control Register Functions
Bit Name | Description | |
---|---|---|
RBUF | Output amplifier configuration control. | |
Setting | Function | |
0 | Internal amplifier powered up. | |
1 (default) | Internal amplifier powered down. | |
OPGND | Output ground clamp control. | |
Setting | Function | |
0 | DAC output clamp to ground removed and DAC placed in normal mode. | |
1 (default) | DAC output clamped to ground and DAC placed in tristate mode. | |
DACTRI | DAC tristate control. | |
Setting | Function | |
0 | DAC in normal operating mode. | |
1 (default) | DAC in tristate mode. | |
BIN/2sC | DAC register coding selection. | |
Setting | Function | |
0 (default) | DAC register uses twos complement coding. | |
1 | DAC register uses offset binary coding. | |
SDODIS | SDO pin enable/disable control. | |
Setting | Function | |
0 (default) | SDO pin enabled. | |
1 | SDO pin disabled (tristate). | |
R/ | Read/write select bit. | |
Setting | Function | |
0 | AD5760/AD5780/AD5790 addressed for a write operation. | |
1 | AD5760/AD5780/AD5790 addressed for a read operation. |
Figure 5. Software Control Register
Table 5. Software Control Register Functions
Bit Name | Description |
---|---|
LDAC1 | Setting this bit to 1 updates the DAC register and, consequently, the DAC output. |
CLR2 | Setting this bit to 1 sets the DAC register to a user defined value and updates the DAC output. |
RESET | Setting this bit to 1 returns the AD5760/AD5780/AD5790 device to its power-on state. |
1 The LDAC function has no effect when the pin is low. Refer to Table 2 in the Hardware Control Pins Truth Table section for further details.
2 The CLR function has no effect when the pin is low. Refer to Table 2 in the Hardware Control Pins Truth Table section for further details.
where:
VREFN is the negative voltage applied at the VREFN input pin.
VREFP is the positive voltage applied at the VREFP input pin.
D is the 16-bit (AD5760), 18-bit (AD5780), or 20-bit (AD5790) code programmed to the DAC.
N is the number of bits.
To initialize the part,
Write the following over the serial interface: 0010 0000 0000 0000 0001 0010 (R/ bit, three register address bits, 20 data bits).
See Table 6 and Figure 6.
Table 6. Bit Settings to Initialize and Write to the Part
Bit(s) | Bit Name | Setting | Description |
---|---|---|---|
23 | R/ | 0 | AD5760/AD5780/AD5790 addressed for a write operation |
[22:20] | C2, C1, C0 | 010 | Write to the control register |
5 | SDODIS | 0 | The SDO pin enabled for future readings from the part |
4 | BIN/2sC | 1 | Offset binary coding |
3 | DACTRI | 0 | Place the DAC in normal operating mode |
2 | OPGND | 0 | Remove the DAC output clamp to ground |
1 | RBUF | 1 | The internal amplifier powered down |
To write in binary coding, set BIN/2sC = 1.
The default coding is twos complement. The same 24-bit data impacts the values that the user writes to or reads from the part in a different way depending on the coding selected. The user must verify the coding used by writing to the control register or reading back from it.
Figure 6. Initializing the Part
To write a midscale code to the DAC register,
The 24-bit data to write over the serial interface is as follows:
16-bit AD5760: 0001 1000 0000 0000 0000 XXXX
18-bit AD5780: 0001 1000 0000 0000 0000 00XX
20-bit AD5790: 0001 1000 0000 0000 0000 0000
where X = don't care.
See Table 7 and Figure 7.
Table 7. Bit Settings to Write to DAC Register
Figure 7. Writing to the DAC Register
To define the value at which the DAC output is set when the pin or CLR bit in the software control register is asserted, write the desired code to the clearcode register.
For a full-scale clear code, write the following over the serial interface:
16-bit AD5760: 0011 1111 1111 1111 1111 XXXX
18-bit AD5780: 0011 1111 1111 1111 1111 11XX
20-bit AD5790: 0011 1111 1111 1111 1111 1111
where X = don't care.
See Figure 8.
Figure 8. Writing Full-Scale Code to the Clearcode Register
Set the CLR bit to a Logic 1 to set the DAC register to a user defined value and update the DAC output.
Write the following over the serial interface: 0100 0000 0000 0000 0000 0010
The user should see the DAC output value change to full-scale code.
See Figure 9.
Figure 9. Clearing the Part to a User Defined Value
To confirm the clearcode value written to the part, read the data from the clearcode register (full scale for this example).
Write the following over the serial interface:
1011 XXXX XXXX XXXX XXXX XXXX.
where X = don't care.
See Figure 10.
Note that this action is a read function. Therefore, set the R/ bit = 1.
D19 to D0, the data bits, are don't care bits because the intention is to read from the part and not to write to the part.
Figure 10. Reading from the Clearcode Register