Wiki

This version (24 Dec 2021 11:54) was approved by Darius B.The Previously approved version (18 Mar 2021 09:06) is available.Diff

TINYIIOD demo

TINYIIOD demo is a standard example, provided in most no-OS projects, that launches a TINYIIOD server on the board so that the user may connect to it via an IIO client. Using iio-oscilloscope, the user can configure the DAC and view the ADC data on a plot.

To build the TINYIIOD demo, add the following flag when invoking make which will build the tinyiiod server and the IIO section of the driver.

make TINYIIOD=y

To run the TINYIIOD demo, first connect to the board via UART to see the runtime output messages with the following settings:

Baud Rate: 115200bps
Data: 8 bit
Parity: None
Stop bits: 1 bit
Flow Control: none

Please note that for proper message display, you may need to convert all LF characters to CRLF, if your serial terminal supports it.

With a serial terminal correctly configured and listening to incoming messages, launch the application (make run or click the debug button in your SDK). Runtime messages specific to the application will apear on your serial terminal screen, and eventually the following message is printed:

Running TinyIIOD server...
If successful, you may connect an IIO client application by:
1. Disconnecting the serial terminal you use to view this message.
2. Connecting the IIO client application using the serial backend configured as shown:
	Baudrate: 921600
	Data size: 8 bits
	Parity: none
	Stop bits: 1
	Flow control: none

This message implies a TINYIIOD server is being run and you may connect to it using a serial-backend enabled iio-oscilloscope and with the settings indicated at the serial terminal.

resources/no-os/tinyiiod_demo.txt · Last modified: 24 Dec 2021 11:53 by Darius B