Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:no-os:build [19 Apr 2022 13:45] – Cygwin warning Darius B | resources:no-os:build [06 May 2022 15:12] – Ciprian Regus |
---|
* Install [[https://www.st.com/en/development-tools/stm32cubemx.html|stm32cubemx]] to default location ''/opt/stm32cubemx''. If you'd rather install it at a different location, run ''export STM32CUBEMX=/path/to/your/stm32cubemx'' in the terminal used for building. | * Install [[https://www.st.com/en/development-tools/stm32cubemx.html|stm32cubemx]] to default location ''/opt/stm32cubemx''. If you'd rather install it at a different location, run ''export STM32CUBEMX=/path/to/your/stm32cubemx'' in the terminal used for building. |
* Install ''java'' (openjdk-11), ''sed'' and ''head'' (if not already present, they normally are). | * Install ''java'' (openjdk-11), ''sed'' and ''head'' (if not already present, they normally are). |
| </hidden> |
| |
| <hidden Maxim (Click to expand)> |
| * Install the [[maxim>en/design/software-description.html/swpart=SFW0018720A|Maxim Micros SDK]]. |
| * Set the MAXIM_LIBRARIES environment variable to the MaximSDK/Libraries path (the default should be ~/MaximSDK/Libraries). |
| * For visual debugging and building, install ''Visual Studio Code'', and the ''Cortex-Debug'' extension. |
</hidden> | </hidden> |
| |
C:\Xilinx\SDK\2018.3\gnuwin\bin | C:\Xilinx\SDK\2018.3\gnuwin\bin |
</code> | </code> |
| </hidden> |
| |
| <hidden Maxim (Click to expand)> |
| * Install the [[maxim>en/design/software-description.html/swpart=SFW0010820A|Maxim Micros SDK]]. |
| * Set the MAXIM_LIBRARIES environment variable to the MaximSDK\Libraries path (the default should be C:\MaximSDK\Libraries). |
| * For visual debugging and building, install ''Visual Studio Code'', and the ''Cortex-Debug'' extension. |
</hidden> | </hidden> |
| |
$ make HARDWARE=path/to/file.hdf | $ make HARDWARE=path/to/file.hdf |
</code> | </code> |
| </hidden> |
| |
| <hidden Maxim (Click to expand)> |
| To build a project, type: |
| <code> |
| make PLATFORM=maxim TARGET=... |
| </code> |
| The ''TARGET'' specifies the chip for which the project is built. If it is missing, ''max32660'' will be used. At the moment, the available targets are: ''max32650'', ''max32655'' and ''max32660''. |
</hidden> | </hidden> |
| |
> make | > make |
</code> | </code> |
| </hidden> |
| |
| <hidden Maxim (Click to expand)> |
| To build a project, type: |
| <code> |
| make PLATFORM=maxim TARGET=... |
| </code> |
| The ''TARGET'' specifies the chip for which the project is built. If it is missing, ''max32660'' will be used. At the moment, the available targets are: ''max32650'', ''max32655'' and ''max32660''. |
</hidden> | </hidden> |
| |