Wiki

This version (08 Jul 2022 08:30) is a draft.
Approvals: 0/1
The Previously approved version (06 May 2022 15:12) is available.Diff

NO-OS Project Build Guide

NOTE: This build guide is valid for the projects found in the no-OS/projects folder. If your project resides elsewhere under the no-OS repository tree, it is a legacy project. A build guide for legacy projects can be found Build no-OS with GNU make.

Clone NO-OS with the --recursive flag:

git clone --recursive https://github.com/analogdevicesinc/no-OS

If however you've already cloned NO-OS without the --recursive flag, you may initialize all the submodules in an existing NO-OS clone with:

git submodule update --recursive --init

Build Prerequisites

Prior to building a no-OS project, it is required to set up some environment variables so that the build process may find the necessary tools (compiler, linker, SDK etc.).

Use the following commands to prepare your environment for building no-OS projects:

Linux (Click to expand)

Linux (Click to expand)

Intel (Click to expand)

Intel (Click to expand)

Assuming the SDK is installed at this path:

/path/to/intel
└── intelFPGA
    └── 18.1

Run:

$ source no-OS/tools/scripts/platform/intel/environment.sh /path/to/intel/intelFPGA 18.1

Xilinx (Click to expand)

Xilinx (Click to expand)

Assuming the Vitis is installed at this path:

/path/to/xilinx
├── DocNav
├── Downloads
├── SDK
│   └── 2019.1
└── Vitis
    └── 2021.1

When using no-OS master branch, run:

$ source /path/to/xilinx/Vitis/2021.1/settings64.sh

When using no-OS 2019_R2 branch, run:

$ source /path/to/xilinx/SDK/2019.1/settings64.sh

For more information, consult the support/answers/47821.html.

STM32 (Click to expand)

STM32 (Click to expand)

  • Install stm32cubeide to default location /opt/stm32cubeide. If you'd rather install it at a different location, run export STM32CUBEIDE=/path/to/your/stm32cubeide in the terminal used for building.
  • Install stm32cubemx to default location /opt/stm32cubemx. If you'd rather install it at a different location, run export STM32CUBEMX=/path/to/your/stm32cubemx in the terminal used for building.
  • Install java (openjdk-11), sed and head (if not already present, they normally are).

Maxim (Click to expand)

Maxim (Click to expand)

  • Install the Maxim Micros SDK.
  • Set the MAXIM_LIBRARIES environment variable to the MaximSDK/Libraries path (the default should be ~/MaximSDK/Libraries).
  • For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

Pico (Click to expand)

Pico (Click to expand)

  • Set the PICO_SDK_PATH environment variable to the pico-sdk cloned repository path.
  • Install the J-Link software
  • Set the JLINK_SERVER_PATH environment variable to the JLinkGDBServerCLExe path (the default path should be /opt/SEGGER/JLink/JLinkGDBServerCLExe).
  • For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

Please install all the necessary packs locally and then manually import them in CrossCore

Common Issues with environment setup:

  • Makefiles searches for the CCES_HOME in its default installation directory. It may happen that multiple version are installed and may not work. To select a CCES_HOME run export CCES_HOME=/opt/analog/cces/2.10.0

Windows (Click to expand)

Windows (Click to expand)

Use cmd or PowerShell. Cygwin is not supported.

Intel (Click to expand)

Intel (Click to expand)

Assuming the SDK is installed at this path:

C:\
└── intelFPGA
    └── 18.1

Run:

> .\no-OS\tools\scripts\platform\altera\environment.bat C:\intelFpga 18.1

Xilinx (Click to expand)

Xilinx (Click to expand)

Assuming the Vitis is installed at this path:

C:\Xilinx
├── DocNav
├── Downloads
├── SDK
│   └── 2019.1
└── Vitis
    └── 2021.1

When using no-OS master branch, run:

> C:\Xilinx\Vitis\2021.1\settings64.bat

When using no-OS 2019_R2 branch, run:

> C:\Xilinx\SDK\2019.1\settings64.bat

For more information, consult the Xilinx support support/answers/47821.html.

Note that Xilinx SDK versions 2018.3 or earlier don't properly set up the Windows PATH so that you may use make command provided with the SDK from the shell.

If this is the case, please manually add the following to your Windows PATH or install make for Windows of your choice:

C:\Xilinx\SDK\2018.3\gnuwin\bin

Maxim (Click to expand)

Maxim (Click to expand)

  • Install the Maxim Micros SDK.
  • Set the MAXIM_LIBRARIES environment variable to the MaximSDK\Libraries path (the default should be C:\MaximSDK\Libraries).
  • For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

Please install all the necessary packs locally and then manually import them in CrossCore

Common Issues with environment setup:

  • Makefiles searches for the CCES_HOME in its default installation directory. It may happen that multiple version are installed and may not work. To select a CCES_HOME run set CCES_HOME=c:\Analog Devices\CrossCore Embedded Studio 2.10.0
If using PowerShell instead of cmd, open another shell instance after running the above scripts.

Building a project

Go in the project directory that should be built.

Linux (Click to expand)

Linux (Click to expand)

$ cd no-OS/projects/project_name/
$ tree
.
├── builds.json
├── Makefile
├── src
└── src.mk

Intel (Click to expand)

Intel (Click to expand)

Copy the .sof and .sopcinfo to the project folder.

$ ls
Makefile  profiles  src  src.mk  system_bd.sopcinfo  adrv9009_a10gx.sof	
$ make

# Alternatively you may select a .sopcinfo file explicitly by:
$ make HARDWARE=path/to/system_bd.sopcinfo

Xilinx (Click to expand)

Xilinx (Click to expand)

Copy the .hdf in the project folder.

$ ls
Makefile  profiles  src  src.mk system_top.hdf
$ make

# Alternatively you may select an .hdf file explicitly by:
$ make HARDWARE=path/to/file.hdf

Maxim (Click to expand)

Maxim (Click to expand)

To build a project, type:

make PLATFORM=maxim TARGET=...

The TARGET specifies the chip for which the project is built. If it is missing, max32660 will be used. At the moment, the available targets are: max32650, max32655 and max32660.

STM32 (Click to expand)

STM32 (Click to expand)

Make sure you have the .ioc file in the project directory, then type:

$ make

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

The ADuCM3029 projects also contain a pinmux_config.c file which contains pin configuration instructions.

# build an ADuCM3029-only project
$ make

# if the platform autodetection picks the wrong platform, explicitly specify the PLATFORM
$ make PLATFORM=aducm3029

Windows (Click to expand)

Windows (Click to expand)

CMD needs to be run with administrative privileges to create a project.

If this is not possible, check the standalone section.

> cd .\no-OS\projects\project_name\

It should contain make-related files and source files:

.\no-OS\projects\project_name\
├── builds.json
├── Makefile
├── src
└── src.mk

Intel (Click to expand)

Intel (Click to expand)

Copy the .sof and .sopcinfo to the project folder and run:

.\no-OS\projects\adrv9009\
├── Makefile
├── profiles
├── src
├── src.mk
├── system_bd.sopcinfo
└── adrv9009_a10gx.sof

> make

Xilinx (Click to expand)

Xilinx (Click to expand)

Copy the .hdf to the project folder and run:

.\no-OS\projects\adrv9009\
├── Makefile
├── profiles
├── src
├── src.mk
└── system_top.hdf

> make

Maxim (Click to expand)

Maxim (Click to expand)

To build a project, type:

make PLATFORM=maxim TARGET=...

The TARGET specifies the chip for which the project is built. If it is missing, max32660 will be used. At the moment, the available targets are: max32650, max32655 and max32660.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

The ADuCM3029 projects also contain a pinmux_config.c file which contains pin configuration instructions.

# build an ADuCM3029-only project
> make

# if the platform autodetection picks the wrong platform, explicitly specify the PLATFORM
> make PLATFORM=aducm3029

The build process creates a build directory in the project folder:

build
├── app
├── bsp
├── obj
├── release.elf
└── tmp

Running/Debugging

Once the .elf or .hex file has been generated, make sure the board is powered on, JTAG cable connected and use the following commands to upload the program to the board or debug.

Uploading the binary to target is generically achieved with:

$ make run

Use the following command to launch the SDK associated to the used platform in order to be able to debug graphically by clicking the debug button:

$ make sdkopen

Fore more details about the available make rules, check out this page.

resources/no-os/build.txt · Last modified: 08 Jul 2022 08:30 by Ramona Bolboaca