Clone NO-OS with the --recursive
flag:
git clone --recursive https://github.com/analogdevicesinc/no-OS
If however you've already cloned NO-OS without the --recursive
flag, you may initialize all the submodules in an existing NO-OS clone with:
git submodule update --recursive --init
Prior to building a no-OS project, it is required to set up some environment variables so that the build process may find the necessary tools (compiler, linker, SDK etc.).
Use the following commands to prepare your environment for building no-OS projects:
Go in the project directory that should be built.
The build process creates a build directory in the project folder:
build ├── app ├── bsp ├── obj ├── release.elf └── tmp
Once the .elf
or .hex
file has been generated, make sure the board is powered on, JTAG cable connected and use the following commands to upload the program to the board or debug.
Uploading the binary to target is generically achieved with:
$ make run
Use the following command to launch the SDK associated to the used platform in order to be able to debug graphically by clicking the debug button:
$ make sdkopen
Fore more details about the available make rules, check out this page.