This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [29 Mar 2013 11:00] Alexandru.Tofan [Running Demo (SDK) Program] |
resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [09 Jan 2021 00:57] Robin Getz user interwiki links |
||
---|---|---|---|
Line 4: | Line 4: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] | + | * [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|Pmod-ACL (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|Pmod-ACL (Digilent)]] | ||
* [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-GYRO2|Pmod-GYRO2 (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-GYRO2|Pmod-GYRO2 (Digilent)]] | ||
Line 15: | Line 15: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm]] for details. | + | <WRAP round 80% tip> |
+ | \\ | ||
+ | If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm]] for details. | ||
</WRAP> | </WRAP> | ||
Line 32: | Line 34: | ||
On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | ||
- | <WRAP important> | + | <WRAP round 80% important> |
* Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | * Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | ||
* Connecting the PmodACL to the board with an extension cable provides ease of use. | * Connecting the PmodACL to the board with an extension cable provides ease of use. | ||
Line 39: | Line 41: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download 50%> | + | <WRAP round download 80%> |
+ | \\ | ||
{{:resources:fpga:xilinx:pmod:ADXRS453_ADXL345.zip|Reference design source code}} | {{:resources:fpga:xilinx:pmod:ADXRS453_ADXL345.zip|Reference design source code}} | ||
</WRAP> | </WRAP> |