Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:xilinx:pmod:ad7780 [20 Nov 2015 13:41]
Lars-Peter Clausen hide linux, it is not supported at the moment
resources:fpga:xilinx:pmod:ad7780 [09 Jan 2021 00:49]
Robin Getz user interwiki links
Line 6: Line 6:
  
 **HW Platform(s):​** ​ **HW Platform(s):​** ​
-   * [[http://www.xilinx.com/products/​boards-and-kits/​AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] ​+   * [[xilinx>products/​boards-and-kits/​AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] ​
    * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]]    * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]]
    * [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx|Avnet ZedBoard]] \\    * [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx|Avnet ZedBoard]] \\
Line 15: Line 15:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://www.xilinx.com/products/​boards-and-kits/​AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]]+  * [[xilinx>products/​boards-and-kits/​AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]]
   * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]]  ​   * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]]  ​
   * [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx|Avnet ZedBoard]] ​   * [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx|Avnet ZedBoard]] ​
Line 26: Line 26:
 ==== Running Demo (SDK) Program ==== ==== Running Demo (SDK) Program ====
  
-<WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/​boards-and-kits/​AES-S6MB-LX9.htm]] for details.\\+<WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/​boards-and-kits/​AES-S6MB-LX9.htm]] for details.\\
 If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3]] for details.\\ If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://​www.digilentinc.com/​Products/​Detail.cfm?​NavPath=2,​400,​897&​Prod=NEXYS3]] for details.\\
 If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx]] for details.</​WRAP>​ If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http://​www.em.avnet.com/​en-us/​design/​drc/​Pages/​Zedboard.aspx]] for details.</​WRAP>​
Line 159: Line 159:
     * Download the project libraries: [[https://​github.com/​analogdevicesinc/​fpgahdl_xilinx/​tree/​master/​cf_lib|Required Project Libraries]]\\     * Download the project libraries: [[https://​github.com/​analogdevicesinc/​fpgahdl_xilinx/​tree/​master/​cf_lib|Required Project Libraries]]\\
     * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step     * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step
-        * [[http://​wiki.analog.com/​resources/​tools-software/​linux-drivers/​platforms/​zynq?​s=adv7511&​s=linux|Linux with HDMI video output on the ZED and ZC702]].+        * [[/​resources/​tools-software/​linux-drivers/​platforms/​zynq?​s=adv7511&​s=linux|Linux with HDMI video output on the ZED and ZC702]].
  
 Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board.
Line 214: Line 214:
  
 Install the ADI IIO Oscilloscope using the instructions from the following wiki page: Install the ADI IIO Oscilloscope using the instructions from the following wiki page:
-    * [[http://​wiki.analog.com/​resources/​tools-software/​linux-software/​iio_oscilloscope|IIO Oscilloscope]]+    * [[/​resources/​tools-software/​linux-software/​iio_oscilloscope|IIO Oscilloscope]]
  
 Launch the ADI IIO Oscilloscope. Launch the ADI IIO Oscilloscope.
resources/fpga/xilinx/pmod/ad7780.txt · Last modified: 09 Jan 2021 00:49 by Robin Getz