Wiki

This version is outdated by a newer approved version.DiffThis version (06 Aug 2012 16:29) is a draft.
Approvals: 0/1

This is an old revision of the document!


AD7303 Pmod Xilinx FPGA Reference Design

Introduction

The AD7303 is a dual, 8-bit voltage out DAC that operates from a single 2.7V to 5.5V supply. Its on-chip precision output buffers allow the DAC outputs to swing rail-to-rail. This device uses a versatile 3-wire serial interface that operates at clock rates up to 30 MHz, and is compatible with QSPIm SPI, microwire and digital signal processor interface standards.

Two reference designs are available for this part:

  • A design which demonstrates how to acquire a signal and reproduce it using Digilent PmodAD1 and PmodDA1. Four types of waveforms (Square, Sine, Sawtooth and Triangle) are generated using the AD7303 DAC present on the PmodDA1 board. Each waveform has a period of 25 ms, and lasts for 25 s (1000 periods). A loopback cable is connected between the output of the AD7303 DAC and the input of the AD7476 ADC present on the PmodAD1 board. The Xilinx ChipScope Analyzer tool is used to verify the digitized waveforms.

AD7303 Pmod Reference Design

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).

Required Hardware

Required Software

  • Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack).
  • A UART terminal (Tera Term/Hyperterminal), Baud rate 115200 for the Avnet LX-9 Microboard or 9600 for the Digilent Nexys™3 Board.

Running Demo (SDK) Program

If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.
If you are not familiar with Nexys™3 and/or Xilix tools, please visit
http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.

Extract the project from the archive file (AD7303_<board_name>.zip) to the location you desire.

Avnet LX9 MicroBoard Setup

To begin, connect the PmodDA1 to J4 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board.

PmodDA1 and LX-9

Digilent Nexys™3 Spartan-6 FPGA Board

To begin, connect the PmodDA1 to JA connector of Nexys™3 board, pins JA1 to JA6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board.

PmodDA1 and Nexys™3

FPGA Configuration

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Connect an oscilloscope to the outputs of the PmodDA1 and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../ad7303/sw/AD7303.bit).

If programming was successful, the Main Menu will apear in your UART terminal, as seen in the picture below. There are 2 options:

  • Press [1] to select Fixed Value Mode.
  • Press [2] to select Waveform Generation Mode.

Main Menu

When entering Fixed Value Mode, DAC selection is automatically activated. Selecting the DAC is done by pressing [1] to [4].

Fixed Value Mode

Fixed Value Mode allows entering a value between 0x00 and 0xFF, value that will be programmed in the DAC. If the number of input characters is less than 2 (e.g. f or 7), the [Enter] key must be pressed in order to validate the input. If 2 characters are input, the value is automatically validated (in order to prevent entering more than 2 characters). Pressing the [s] key at any time will enter DAC Selection Mode.

UART messeges

Pressing the [q] key at any time exits the Fixed Value (or Waveform Generation) Mode and displays the Main Menu again.

Returning to Menu

When entering Waveform Generation Mode, DAC selection is automatically activated. Selecting the DAC is done by pressing [1] to [4].

Waveform Generation Mode

Waveform Generation Mode allows selecting between 4 types of waveforms: Square, Triangle, Sawtooth and Sine waveforms. Changing between the 4 is done by pressing [1] to [4] on the keyboard. Pressing [s] at any time will enter DAC Selection Mode. Pressing [q] at any time will return to the Main Menu.

Selecting Waveform type

Using the reference design

Functional Description

The reference design is a simple SPI interface with two MOSI pins for the PmodDA1. The software programs the device sending an 8-bit configuration value followed by 8-bit data value.

The hardware SPI access allows writing data to the AD7303, using a single CS and SCLK pins, and two MOSI pins (PmodDA1 contains two AD7303 Integrated Circuits, which share the same CS and SCLK pins, but have separate MOSI pins).

  • Connecting the PmodDA1 to the boards using an extension cable provides ease of use.
  • UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board.

Downloads

AD7303 Pmod and AD7476 Pmod Reference Design

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system.

Required Hardware

Required Software

Running Demo (SDK) Program


If you are not familiar with Nexys3 and/or Xilix tools, please visit
http://digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.

To begin, connect the PmodAD1 to JA1 connector of Nexys3 board, pins 1 to 6 (see image below) and the PmodDA1 to JB1 connector of Nexys3 board, pins 1 to 6. You can use an extension cable for ease of use. Connect the USB cables from the PC to the board.

 Connecting Pmods to Nexys3

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Program the FPGA using the download.bit file provided in the project *.zip archive, located in the “sw” folder (../ad7303_ad7476/sw/download.bit).

Programming FPGA in IMPACT

Start the ChipScope Pro Analyzer provided with the Xilinx ISE Design Suite 13.2 and load the project Nexys3_ChipScope_Demo.cpj located in the “chipscope” folder (../ad7303_ad7476/chipscope/Nexys3_ChipScope_Demo.cpj). Click the Open Cable/Search JTAG Chain button and afterwards double click Bus Plot and select Repetitive Trigger Run Mode. Click the Apply Settings and Arm Trigger button. On the main screen you will se the waveforms change once every 25 seconds, between Sine, Square, Sawtooth and Triangle waveforms. Each waveform has a period of 25ms. You can compare the waveform displayed in ChipScope Pro with the waveform displayed on an oscilloscope from the DAC output.

Viewing Waveforms in ChipScope Pro

  • Connecting the Pmod-AD1 and/or Pmod-DA1 to the Nexys3 Board using an extension cable provides ease of use.
  • UART must be set to 57600 baudrate.
  • The reference voltage for both the AD7476A and AD7303 is 3.3V (if using Nexys3 Board).
  • A loopback cable is connected between the output of the AD7303 DAC (A1 out) and the input of the AD7476 ADC present on the PmodAD1 board (pin1 in = A0 in).

Downloads

10 Apr 2012 12:28 · Alexandru.Tofan

More information

resources/fpga/xilinx/pmod/ad7303.1344263359.txt.gz · Last modified: 06 Aug 2012 16:29 (external edit)