Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (10 Feb 2012 13:34) was approved by Andrei Cozma.

This is an old revision of the document!


AD7193 Xilinx Pmod FPGA Reference Design

Introduction

The AD7193 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog-to-digital converter (ADC). The on-chip low noise gain stage means that signals of small amplitude can interface directly to the ADC. The device can be configured to have four differential inputs or eight pseudo differential inputs. The on-chip channel sequencer allows several channels to be enabled simultaneously, and the AD7193 sequentially converts on each enabled channel, simplifying communication with the part. The on-chip 4.92 MHz clock can be used as the clock source to the ADC or, alternatively, an external clock or crystal can be used. The output data rate from the part can be varied from 4.7 Hz to 4.8 kHz.

HW Platform(s): Spartan-6 LX9 Microboard (Avnet) Pmod-AD5 (Digilent)
System: Microblaze, AXI, UART

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).

Required Hardware

  • LX9 microboard
  • Pmod-AD5

Required Software

  • Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack).
  • A UART terminal (Tera Term/Hyperterminal), Baud rate 57600.

Running Demo (SDK) Program

If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.

Extract the project from the archive file (AD7193.zip) to the location you desire.

To begin, connect the Pmod-AD5 to J5 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board.

Pmod-AD5 and LX-9

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set to 57600 baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../ad7193/sw/AD7193.bit).

Programming FPGA in IMPACT

If programming was successful, you should be seeing messages appear on the terminal window as shown in the figures below. After programming the AD7193, the program will display the values of all internal registers. After that, it will go through 3 Demo Modes: Read Voltage Values referenced to AINCOM, Read Differential Voltage Values and Read Die Temperature Value.

UART messeges UART messeges UART messeges UART messeges

Using the reference design

Functional Description

The reference design is a custom SPI Interface, containing CS, SCLK, MISO, MOSI, but also a GPIO to read the RDY status on the MISO line. The information is displayed on UART.

The hardware SPI access allows sending and receiving data from the AD7193, programming its internal registers in order to decide which channels should be converted corresponding to AINCOM or its own differential pair, what GAIN, sampling frequency, etc.

  • Connecting the Pmod-AD5 to the LX-9 Board using an extension cable provides ease of use.
  • UART must be set to 57600 baudrate.
  • Reference voltage is 2.5V

Downloads

More information

resources/fpga/xilinx/pmod/ad7193.1328877241.txt.gz · Last modified: 10 Feb 2012 13:34 by Andrei Cozma