Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
resources:fpga:xilinx:pmod:ad7193 [10 Feb 2012 13:34]
Andrei Cozma Approved
resources:fpga:xilinx:pmod:ad7193 [10 Feb 2012 14:31]
Alexandru Tofan [Functional Description]
Line 59: Line 59:
   * UART must be set to 57600 baudrate.   * UART must be set to 57600 baudrate.
   * Reference voltage is 2.5V   * Reference voltage is 2.5V
 +  * If using Xilinx Software Development Kit integrated Console as a Hyperterminal clinet, please uncomment all the commented **getchar();​** in main.c, because the Console sees [Enter] as 2 consecutive keypresses, so 2 getchar(); are required. If using Tera Term or other similar software, do not modify anything. ​
 </​note>​ </​note>​
  
resources/fpga/xilinx/pmod/ad7193.txt · Last modified: 09 Jan 2021 00:49 by Robin Getz