Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
resources:fpga:xilinx:pmod:ad7091r [10 Dec 2012 15:52] – Download Wrapper Alexandru.Tofanresources:fpga:xilinx:pmod:ad7091r [03 Jan 2013 20:42] – external edit
Line 26: Line 26:
 ==== Running Demo (SDK) Program ==== ==== Running Demo (SDK) Program ====
  
-<note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm]] for details.\\+<WRAP tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm]] for details.\\
 If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3]] for details. If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3]] for details.
-</note>+</WRAP>
 Extract the project from the archive file (AD7091R_<board_name>.zip) to the location you desire.  Extract the project from the archive file (AD7091R_<board_name>.zip) to the location you desire. 
  
Line 61: Line 61:
 The hardware SPI access allows receiving data from the AD7091R. The hardware SPI access allows receiving data from the AD7091R.
  
-<note important>+<WRAP important>
   * Connecting the PmodAD6 to the boards using an extension cable provides ease of use.   * Connecting the PmodAD6 to the boards using an extension cable provides ease of use.
   * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board.   * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board.
   * Reference voltage is 2.5V   * Reference voltage is 2.5V
-</note>+</WRAP>
  
  
resources/fpga/xilinx/pmod/ad7091r.txt · Last modified: 09 Jan 2021 00:49 by Robin Getz