This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:fpga:xilinx:pmod:ad7091r [20 Nov 2015 13:43] Lars-Peter Clausen hide linux, it is not supported at the moment |
resources:fpga:xilinx:pmod:ad7091r [09 Jan 2021 00:49] Robin Getz user interwiki links |
||
---|---|---|---|
Line 6: | Line 6: | ||
**HW Platform(s):** | **HW Platform(s):** | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] | + | * [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] | ||
* [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] \\ | * [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] \\ | ||
Line 15: | Line 15: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] | + | * [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm|Spartan-6 LX9 Microboard (Avnet)]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] | * [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3|Nexys™3 Spartan-6 FPGA Board (Digilent)]] | ||
* [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] | * [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx|Avnet ZedBoard]] | ||
Line 26: | Line 26: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm]] for details.\\ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/boards-and-kits/AES-S6MB-LX9.htm]] for details.\\ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3]] for details.\\ | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3]] for details.\\ | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx]] for details.</WRAP> | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx]] for details.</WRAP> | ||
Line 135: | Line 135: | ||
* Download the project libraries: [[https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_lib|Required Project Libraries]]\\ | * Download the project libraries: [[https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_lib|Required Project Libraries]]\\ | ||
* Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | ||
- | * [[http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq?s=adv7511&s=linux|Linux with HDMI video output on the ZED and ZC702]]. | + | * [[/resources/tools-software/linux-drivers/platforms/zynq?s=adv7511&s=linux|Linux with HDMI video output on the ZED and ZC702]]. |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
Line 196: | Line 196: | ||
Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
- | * [[http://wiki.analog.com/resources/tools-software/linux-software/iio_oscilloscope|IIO Oscilloscope]] | + | * [[/resources/tools-software/linux-software/iio_oscilloscope|IIO Oscilloscope]] |
Launch the ADI IIO Oscilloscope. | Launch the ADI IIO Oscilloscope. |