This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:ad5628 [16 Oct 2013 13:27] – adding linux (in progress) Alexandru.Tofan | resources:fpga:xilinx:pmod:ad5628 [30 Oct 2013 10:05] – [Preparing the SD Card] Alexandru.Tofan | ||
---|---|---|---|
Line 186: | Line 186: | ||
There are 2 ways to test the driver. | There are 2 ways to test the driver. | ||
* Using the terminal window | * Using the terminal window | ||
- | * Using the ADI IIO Oscilloscope | + | * Using a serial terminal |
===== Using the terminal window ===== | ===== Using the terminal window ===== |