Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:fpga:xilinx:interposer:ucprobe3_common [13 Jul 2012 13:41]
Alexandru.Tofan created
resources:fpga:xilinx:interposer:ucprobe3_common [03 Jan 2013 20:42] (current)
Line 1: Line 1:
 ===== Hardware Setup ===== ===== Hardware Setup =====
  
-<note important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</note>+<WRAP important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</WRAP>
  
   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.
Line 17: Line 17:
  
 Select **uC-Probe** options. Select **uC-Probe** options.
-  * Click on the **uC-Probe** icon on the top left portion of the screen. +  * Click on the **File** tab on the top left portion of the screen. 
-  * Click on the **//Options//** button to open the dialog box.+  * Click on the **//Settings//** button to open the dialog box.
  
 {{ :​resources:​fpga:​altera:​bemicro:​ucprobe3optionsbtn.png?​300 }} {{ :​resources:​fpga:​altera:​bemicro:​ucprobe3optionsbtn.png?​300 }}
Line 26: Line 26:
   * Select the **//​RS-232//​** option.   * Select the **//​RS-232//​** option.
  
-{{ :​resources:​fpga:​xilinx:​interposer:​ucprobe3_comm.png?​300 }} +Setup **//​RS-232//​** communication ​setting
- +
-Setup **//​RS-232//​** communication ​settings+
   * Select the **//​RS-232//​** option from the **//​Communication//​** tab.   * Select the **//​RS-232//​** option from the **//​Communication//​** tab.
   * Select the COM port to which the KC705 board is connected.   * Select the COM port to which the KC705 board is connected.
   * Set the Baud Rate to 115200 bps.   * Set the Baud Rate to 115200 bps.
  
-{{ :​resources:​fpga:​xilinx:​interposer:​ucprobe3_rs232.png?300 }}+{{ :​resources:​fpga:​xilinx:​interposer:​ucprobe3_comm.png?300 }}
  
   * Press **//​Apply//​** and **//OK//** to exit the options menu.   * Press **//​Apply//​** and **//OK//** to exit the options menu.
Line 47: Line 45:
 {{ :​resources:​fpga:​altera:​bemicro:​ucprobe3_play.png?​200 }} {{ :​resources:​fpga:​altera:​bemicro:​ucprobe3_play.png?​200 }}
  
-<note tip>  ​+<WRAP tip>  ​
   * In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **//​Stop//​** button and run it again by pressing the **//​Play//​** button.   * In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **//​Stop//​** button and run it again by pressing the **//​Play//​** button.
   * After starting the uC-Probe interface wait until the status of the connection with the board displayed on the bottom of the screen is set to //​**Connected**//​. It is possible to use the interface only after the status is changed to //​**Connected**//​ and the data transfer speed displayed next to the connection status is different than 0.   * After starting the uC-Probe interface wait until the status of the connection with the board displayed on the bottom of the screen is set to //​**Connected**//​. It is possible to use the interface only after the status is changed to //​**Connected**//​ and the data transfer speed displayed next to the connection status is different than 0.
-</note>+</WRAP>
  
resources/fpga/xilinx/interposer/ucprobe3_common.txt · Last modified: 03 Jan 2013 20:42 (external edit)