This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:xilinx:interposer:ucprobe3_common [13 Jul 2012 14:00] – [Configure uC-Probe] Alexandru.Tofan | resources:fpga:xilinx:interposer:ucprobe3_common [03 Jan 2013 20:42] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 45: | Line 45: | ||
{{ : | {{ : | ||
- | <note tip> | + | <WRAP tip> |
* In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **// | * In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **// | ||
* After starting the uC-Probe interface wait until the status of the connection with the board displayed on the bottom of the screen is set to // | * After starting the uC-Probe interface wait until the status of the connection with the board displayed on the bottom of the screen is set to // | ||
- | </note> | + | </WRAP> |