Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.
Launch Tera Term from the Start → All Programs → Tera Term Pro → Tera Term Pro
Select Setup → Serial port… and set the baud rate to 115200.
Select Setup → Terminal.. and enable Local Echo.
After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the Loadapp.bat batch script, which can be found in the LoadApp directory.
If the script threw an error, verify if the Xilinx EDK path specified in the Loadapp.bat script is corresponding with the current install path. If not change it to the correct one.