Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 12:02]
Istvan Csomortani Correct typeos
resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 13:58]
Istvan Csomortani Add title ++Upload Application Software++
Line 22: Line 22:
  
 {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_setup.png?​400 }}  {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_setup.png?​400 }} 
 +
 +===== Upload Application Software =====
  
 After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the //​Loadapp.bat//​ batch script, which can be found in the **LoadApp** directory. After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the //​Loadapp.bat//​ batch script, which can be found in the **LoadApp** directory.
  
 <WRAP tip>If the script threw an error, verify if the Xilinx EDK path specified in the **Loadapp.bat** script is corresponding with the current install path. If not change it to the correct one.</​WRAP>​ <WRAP tip>If the script threw an error, verify if the Xilinx EDK path specified in the **Loadapp.bat** script is corresponding with the current install path. If not change it to the correct one.</​WRAP>​
resources/fpga/xilinx/interposer/terminal_common.txt · Last modified: 02 Jul 2013 13:58 by Istvan Csomortani