This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:cn0271 [13 Jul 2012 15:22] – added archive Alexandru.Tofan | resources:fpga:xilinx:interposer:cn0271 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
* [[adi> | * [[adi> | ||
- | ===== Evaluation Boards | + | ===== Reference Circuits |
- | + | ||
- | * [[adi> | + | |
+ | * [[adi> | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
- | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0271A-SDPZ** Evaluation Board. | + | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0271-SDPZ** Evaluation Board. |
{{ : | {{ : | ||
Line 38: | Line 33: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[adi>/ | + | * [[adi> |
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
- | * [[http:// | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 48: | Line 42: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-CN0271-SDPZ** evaluation board | * **EVAL-CN0271-SDPZ** evaluation board | ||
Line 54: | Line 48: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-CN0271 reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{:resources: | + | \\ |
- | + | * **AD7790 Driver:** https://github.com/ | |
- | The following table presents a short description the reference design archive contents. | + | * **CN0271 Commands:** https:// |
- | + | | |
- | ^ **Folder** ^ **Description** ^ | + | * **EDK KC705 Reference |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </ |
- | | Software | Contains the source files of the software | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | {{page> | + | ===== Hardware setup ===== |
- | ===== Demonstration Project User Interface ===== | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </ | ||
- | The following figure presents | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
+ | | ||
- | {{ : | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-CN0271 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **adcCode? | ||
+ | | **temperature? | ||
+ | | **reset!** | Resets the serial interface with AD7790. | | ||
- | **Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the **// | ||
- | **Section B** is used to acquire data from AD7790. | + | Commands can be executed using a serial terminal connected |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |