This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:fpga:xilinx:interposer:cn0178 [15 Nov 2013 13:50] – changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== CN0178 FMC-SDP Interposer & Evaluation Board / Xilinx KC705 Reference Design ====== | ||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | ===== Reference Circuits ===== | ||
+ | |||
+ | * [[adi> | ||
+ | ====== Overview ====== | ||
+ | |||
+ | This document presents the steps to setup an environment for using the **[[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0178-SDPZ** Evaluation Board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The measurement result is provided as serial data at the output of a 12-bit ADC ([[adi> | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The **EVAL-CN0178-SDP** board contains the circuit to be evaluated, as described in this note. To power the EVAL-CN0178C-SDP evaluation board supply +6V between the +6 V and GND inputs. | ||
+ | |||
+ | ===== More information ===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi>/ | ||
+ | * [[http:// | ||
+ | |||
+ | ====== Getting Started ====== | ||
+ | |||
+ | The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project. | ||
+ | |||
+ | ===== Required Hardware ===== | ||
+ | |||
+ | * [[http:// | ||
+ | * FMC-SDP adapter board | ||
+ | * **EVAL-CN0178-SDPZ** evaluation board | ||
+ | |||
+ | ===== Required Software ===== | ||
+ | |||
+ | * Xilinx ISE 14.6. | ||
+ | * UART Terminal (Termite/ | ||
+ | * The EVAL-CN0178 reference project for Xilinx KC705 FPGA. | ||
+ | |||
+ | |||
+ | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * **AD7466 Driver:** https:// | ||
+ | * **CN0178 Commands:** https:// | ||
+ | * **Xilinx Boards Common Drivers:** https:// | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
+ | </ | ||
+ | ====== Run the Demonstration Project ====== | ||
+ | |||
+ | ===== Hardware setup ===== | ||
+ | |||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </ | ||
+ | |||
+ | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
+ | |||
+ | ===== Reference Project Overview ===== | ||
+ | The following commands were implemented in this version of EVAL-CN0178 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **calibration=** | Makes a four points calibration. Accepted values:\\ power input1(lowest value):\\ -60 .. 0 - first point input power in [dBm].\\ power input2:\\ -60 .. 0 - second point input power in [dBm].\\ power input3:\\ -60 .. 0 - third point input power in [dBm].\\ power input3(highest value):\\ -60 .. 0 - fourth point input power in [dBm]. | | ||
+ | | **pinCalc? | ||
+ | | **error?** | Displays the error associated with the last input power calculation. Accepted values:\\ -60 .. 0 - true input power in [dBm]. | | ||
+ | |||
+ | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. | ||
+ | |||
+ | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. | ||
+ | {{ : | ||
+ | |||
+ | ===== Software Project Setup ===== | ||
+ | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | * [[resources: | ||
+ | {{page> |