Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:adf4002 [19 Nov 2012 18:55]
larsc [Evaluation Boards] fix link
resources:fpga:xilinx:interposer:adf4002 [31 Oct 2013 10:56]
CsomI Fix some typos.
Line 10: Line 10:
 ====== Overview ====== ====== Overview ======
  
-This document presents the steps to setup an environment for using the **[[adi>​ADF4002|EVAL-ADF4002SD1Z]]** evaluation board together with the Xilinx KC705 FPGA boardthe Xilinx Embedded Development Kit (EDK) and the [[http://​micrium.com/​page/​products/​tools/​probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-ADF4002SD1Z Evaluation Board with the Xilinx KC705 board.+This document presents the steps to setup an environment for using the **[[adi>​ADF4002|EVAL-ADF4002SD1Z]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-ADF4002SD1Z Evaluation Board with the Xilinx KC705 board.
  
 {{ :​resources:​fpga:​xilinx:​interposer:​img_adf4001.jpg }} {{ :​resources:​fpga:​xilinx:​interposer:​img_adf4001.jpg }}
Line 28: Line 28:
   * [[adi>/​static/​imported-files/​user_guides/​UG-108.pdf|EVAL-ADF4002SD1Z evaluation board user guide]]   * [[adi>/​static/​imported-files/​user_guides/​UG-108.pdf|EVAL-ADF4002SD1Z evaluation board user guide]]
   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
-  * [[http://​micrium.com/​page/​products/​tools/​probe|Micrium uC-Probe]] 
  
 ====== Getting Started ====== ====== Getting Started ======
Line 42: Line 41:
 ===== Required Software ===== ===== Required Software =====
  
-  * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack)+  * Xilinx ISE 14.6
-  * [[http://micrium.com/​page/​products/​tools/​probe|uC-Probe]] run-time monitoring tool+  * UART Terminal (Termite/Tera Term/Hyperterminal),​ baud rate 115200.
  
 ===== Downloads ===== ===== Downloads =====
 +<WRAP round download 80%>
 +\\
 +  * **ADF4002 Driver:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​device_drivers/​ADF4106
 +  * **ADF4002 Commands:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​device_commands/​ADF4106
 +  * **Xilinx Boards Common Drivers:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​platform_drivers/​Xilinx/​SDP_Common
 +  * **EDK KC705 Reference project:** https://​github.com/​analogdevicesinc/​fpgahdl_xilinx/​tree/​master/​cf_sdp_kc705
 +\\
 +</​WRAP>​
  
-  * {{:​resources:​fpga:​xilinx:​interposer:​adf4002_evalboard.zip|Reference Design Files}}+===== Hardware setup =====
  
-The following table presents a short description ​the reference design archive contents.+<WRAP round important 80%> 
 +\\ 
 +Before connecting ​the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. 
 +</​WRAP>​
  
-**Folder** ^ **Description** ^ +  ​Use the FMC-SDP interposer ​to connect ​the ADI evaluation ​board to the Xilinx ​KC705 board on the FMC LPC connector
-| Bit | Contains ​the KC705 configuration file that can be used to program ​the system for quick evaluation. | +  * Connect ​the JTAG and UART cables ​to the KC705 and power up the FPGA board.
-| Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | +
-| Software | Contains the source files of the software project that will be run by the Microblaze processor.| +
-| uCProbeInterface | Contains ​the uCProbe interface ​and the .elf symbols file used by uC-Probe ​to access data from the Microblaze memory|+
  
-====== Run the Demonstration ​Project ======+===== Reference ​Project ​Overview ​===== 
 +The following commands were implemented in this version of EVAL-ADF4002SD1Z reference project for Xilinx KC705 FPGA board. 
 +^ Command ^ Description ^ 
 +| **help?** | Displays all available commands. | 
 +| **setregister=** | Update the selected latch with the current set ups. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch\\ value:\\ 24 bit values, you can find more information about the registers in the data sheet | 
 +| **getregister?​** | Print the specified latch values in a human readable format. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch | 
 +| **setfrequency=** | Set the VCO frequency. Accepted value:\\ 5 .. 400 - betwwen 5Mhz and 400Mhz | 
 +| **getfrequency?​** | Print the actual VCO frequency. |
  
-{{page>​ucprobe_common}}+Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
  
-===== Demonstration Project User Interface =====+The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. 
 +{{ :​resources:​fpga:​xilinx:​interposer:​Terminal_KC705.jpg?​ }}
  
-The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-ADF4002SD1Z** evaluation board. +===== Software Project Setup ===== 
- +{{page>​import_workspace}}
-{{ :​resources:​fpga:​altera:​bemicro:​adf4002interface.png?​700 }} +
- +
-**Section A** allows for the communication with the board to be activated / deactivated by toggling the //ON/OFF// switch. The //​Activity//​ LED turns green when the communication is active. Before pressing the //ON/OFF// switch, make sure you select the desired //Device Initialization Procedure//​. If the //ON/OFF// switch is set to ON and the //​Activity//​ LED is BLACK it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. +
-The //Error// LED will indicate that the data received on the SDO pin is different than data sent. If the //Function Latch// or //​Initialization Latch// is written, with a different //MUXOUT// value than 6, this LED will be activated. To reset the LED, the board must be deactivated and reactivated,​ case in which the //​Initialization procedure// will set //MUXOUT// to 6. +
- +
-**Sections B to E** allow for configuration of each latch on the **ADF4002**. +
- +
-**Section B** allows for the configuration of the //Reference Counter Latch//. The //LDP// switch will toggle on or off the //Lock Detect Precision// bits. The //TBS// and //ABW// sliders will configure the //Test Mode Bits// and //Anti Backlash Width// bits respectively. The //14 Bit Reference Counter// allows for the configuration of the counter. The last numerical display will display the resulting value in a decimal format. By toggling the //Write// switch in this section, a single write will be performed on the //Reference Counter Latch// with the programmed value. +
- +
-**Section C** allows for the configuration of the //N Counter Latch//. The //CPG// switch toggles the //CP Gain// bit. The //13 Bit N Counter// allows for the configuration of the N counter. The last numerical display in the row will display the resulting value in a decimal format. By toggling the //Write// switch, a single write will be performed on the //N Counter Latch//, with the value displayed.  +
- +
-**Sections D and E** have the same structure. The difference between these two latches is that when the //​Initialization Latch// is programmed, there is an additional internal reset pulse applied to the //R// and //N// counters. This pulse ensures that the //N counter// is at a load point when the //N counter// data is latched, and the device will begin counting in close phase alignment. +
-//PD2// switch toggles the //Power Down 2// pin. The //CS2// and //CS1// sliders will configure the //Current Setting 2// and //Current Setting 1// bits respectively. The //Timer Counter Control// can be configured through the //TCC// slider. Next, the switches configure the //Fastlock Mode//, //Fastlock Enable//, //CP Three-State//​ and //Phase Detector Polarity// bits. The //MUX// slider allows to select what is to be available on the //MUXOUT// pin. By default, at initialization,​ this has the value 6 set, in order to be able to use this pin as SDO. //PD1// switch allows for setting the //Power Down 1// bits. Lastly, the //CR// switch allows for resetting the //R// and //N// counters. +
- +
-===== Troubleshooting ​===== +
- +
-In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: +
-  * Check that the evaluation board is powered as instructed in the board'​s user guide. +
-  * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//​**. +
-  * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again.+
  
 ====== More information ====== ====== More information ======
 {{page>​ez_common}} {{page>​ez_common}}
resources/fpga/xilinx/interposer/adf4002.txt · Last modified: 31 Oct 2013 10:56 by CsomI