This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad9739a [21 Jun 2012 15:57] – changed title to be more meaningful. rejeesh kutty | resources:fpga:xilinx:interposer:ad9739a [20 Dec 2023 11:50] (current) – Add obsolesce notice. Stefan-Robert Raus | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD9739A Evaluation Board, DAC-FMC Interposer & Xilinx Reference Design ====== | ====== AD9739A Evaluation Board, DAC-FMC Interposer & Xilinx Reference Design ====== | ||
+ | <note warning> | ||
+ | Support for the eval-ad9739a is discontinued | ||
+ | </ | ||
+ | |||
===== Introduction ===== | ===== Introduction ===== | ||
The [[adi> | The [[adi> | ||
- | **HW Platform(s): | + | ===== Supported Devices ===== |
- | **System:** Microblaze, AXI, UART | + | |
+ | | ||
+ | * [[adi>en/evaluation/ | ||
+ | |||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | | ||
+ | | ||
+ | | ||
+ | |||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
Line 24: | Line 39: | ||
* Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
* A UART terminal (Tera Term/ | * A UART terminal (Tera Term/ | ||
- | * ADI DPG DAC Software Suite [[http://www.analog.com/en/ | + | * ADI DPG DAC Software Suite [[/resources/eval/dpg/dacsoftwaresuite|available here]]. |
==== Bit file ==== | ==== Bit file ==== | ||
Line 32: | Line 47: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[http:// | ||
- | </ | ||
To begin make the following connections (see image below): | To begin make the following connections (see image below): | ||
Line 89: | Line 102: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | {{: | + | FPGA Referece Designs: |
- | {{: | + | <WRAP round download 80%> |
- | {{: | + | * **ML605 ** {{: |
+ | * **KC705 ** {{: | ||
+ | * **VC707 ** {{: | ||
+ | </ | ||
- | ===== Notes ===== | + | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/ |
- | The following two files are removed from the tar file. | + | <WRAP round help 80%> |
+ | * Questions? [[ez> | ||
+ | </ | ||
- | * pcores/ | ||
- | * pcores/ | ||
- | To use the reference design as it is, re-generate the Xilinx DDS core for a single sine output (16bit) in full range mode. | ||
===== Tar file contents ===== | ===== Tar file contents ===== | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| license.txt | ADI license & copyright information. | | | license.txt | ADI license & copyright information. | | ||
Line 118: | Line 132: | ||
===== More information ===== | ===== More information ===== | ||
- | * [[http:// | + | * [[http:// |
* [[ez> | * [[ez> | ||