Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:fpga:xilinx:interposer:ad9683 [22 Feb 2017 19:42]
Lars-Peter Clausen Canonical spelling of JESD204B
resources:fpga:xilinx:interposer:ad9683 [25 Jan 2021 19:33]
Robin Getz update renesas links after their web site update
Line 7: Line 7:
 ===== Supported Devices ===== ===== Supported Devices =====
  
-  * [[http://​www.analog.com/​en/​analog-to-digital-converters/​ad-converters/​ad9683/​products/​product.html#​product-evaluationkits| AD9683 Evaluation Board]] +  * [[adi>en/​analog-to-digital-converters/​ad-converters/​ad9683/​products/​product.html#​product-evaluationkits| AD9683 Evaluation Board]] 
-  * [[http://​www.analog.com/​en/​evaluation/​eval-adc-fmc-int/​eb.html| High speed ADC FMC interposer]]+  * [[adi>en/​evaluation/​eval-adc-fmc-int/​eb.html| High speed ADC FMC interposer]]
  
 ===== Supported Carriers ===== ===== Supported Carriers =====
Line 161: Line 161:
 </​WRAP>​ </​WRAP>​
  
-Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[http://​wiki.analog.com/​resources/​eval/​user-guides/​ad-fmcomms1-ebz/​reference_hdl|generating Xilinx netlist/​verilog files from xco files]] for details.+Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/​resources/​eval/​user-guides/​ad-fmcomms1-ebz/​reference_hdl|generating Xilinx netlist/​verilog files from xco files]] for details.
  
 <WRAP round help 80%> <WRAP round help 80%>
-  * Questions? [[http://ez.analog.com/​post!input.jspa?​containerType=14&​container=2061|Ask Help & Support]].+  * Questions? [[ez>fpga|Ask Help & Support]].
 </​WRAP>​ </​WRAP>​
  
 ===== Tar file contents ===== ===== Tar file contents =====
  
-The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/​documentation/​dt_edk_edk13-2.htm|Xilinx EDK documentation]] for details.+The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/​documentation/​dt_edk_edk13-2.htm|Xilinx EDK documentation]] for details.
  
 | license.txt | ADI license & copyright information. | | license.txt | ADI license & copyright information. |
Line 182: Line 182:
 ===== More information ===== ===== More information =====
  
-  * [[http://​www.vita.com/​fmc.html|VITA'​s FMC info]]+  * [[http://​www.vita.com/​fmc|VITA'​s FMC info]]
   * [[ez>​community/​fpga|Ask questions about the FPGA reference design]]   * [[ez>​community/​fpga|Ask questions about the FPGA reference design]]
  
  
  
resources/fpga/xilinx/interposer/ad9683.txt · Last modified: 28 Jan 2021 19:14 by Robin Getz