This is an old revision of the document!
The AD9129 is a 14-bit, high performance digital-to-analog converter (DAC) that provides a sample rate of 2.8GSPS. This reference design includes a DDS generator that drives the device. The programming is done via the USB-SPI interface.
The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal, ADI DAC software and the programmer (IMPACT).
To begin make the following connections (see image below):
Setup the clock source to be 2.4GHz/0dBm. After the hardware setup, turn the power on to the ML605 and the AD9129-EBZ boards.
Start ADI- AD9129 SPI program (see screenshot below) and click on “Run Forever” button.
Start IMPACT, and initialze the JTAG chain. The program should recognize the Virtex 6 device. Start a UART terminal (set to 57600 baud rate) and then program the device.
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below.
After DDS is enabled, disable and enable the DLL on the AD9129 SPI interface. You should see the spectrum analyzer displaying a 300MHz tone.
The reference design consists of a DDS module and a lvds interface.
The DDS module consists of a Xilinx IP core and a DDR-DDS. Internally the DDS runs at fDAC/3 clock. The DDR-DDS allows any pattern to be generated in the memory to be driven to the DAC. The output samples are interleaved and driven by the lvds interface.
Please see the regmap.txt file in the pcore directory.
Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See generating Xilinx netlist/verilog files from xco files for details.
The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to Xilinx EDK documentation for details.
license.txt | ADI license & copyright information. |
system.mhs | MHS file. |
system.xmp | XMP file (use this file to build the reference design). |
data/ | UCF file and/or DDR MIG project files. |
docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). |
sw/ | Software (Xilinx SDK) & bit file(s). |
cf_lib/edk/pcores/ | Reference design core file(s) (Xilinx EDK). |