This is an old revision of the document!
AD971x/AD911x-DPG2 FMC Interposer & Evaluation Board / Xilinx ML-605 Reference Design
Supported Devices
Evaluation Boards
Introduction
The AD9114/AD9115/AD9116/AD9117 are pin-compatible dual, 8-/10-/12-/14-bit, low power digital-to-analog converters (DACs) that provide a sample rate of 125 MSPS. These TxDAC® converters are optimized for the transmit signal path of commu-nication systems. All the devices share the same interface, package, and pinout, providing an upward or downward component selection path based on performance, resolution, and cost.
The AD9114/AD9115/AD9116/AD9117 offer exceptional ac and dc performance and support update rates up to 125 MSPS.
The flexible power supply operating range of 1.8 V to 3.3 V and low power dissipation of the AD9114/AD9115/AD9116/AD9117 make them well suited for portable and low power applications.
HW Platform(s): Virtex-6 ML605 (Xilinx), AD9114 Evaluation Board (ADI) / AD9115 Evaluation Board (ADI) / AD9116 Evaluation Board (ADI) / AD9117 Evaluation Board (ADI), DAC FMC Interposer Board (ADI)
System: Microblaze, AXI, UART
Quick Start Guide
The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal, ADI DAC software and the programmer (IMPACT).
Required Hardware
ML605 board
AD911x-DPG2-EBZ board
DAC FMC interposer board
Any PIC ICSP Programmer (
e.g. PICkit 2 or PICkit 3 from Microchip)
Required Software
Bit file
Download the zip file and extract the
AD911x_SPI_Adapter.hex and
AD911x.bit files in the project *.zip archive, located in the “sw” folder (../ad911x/sw/AD911x.bit). (where x is 4,5,6 or 7)
Running Demo (SDK) Program
Extract the project from the archive file (AD911x.zip) to the location you desire.
To begin make the following connections (see image below):
Programming the PIC
Connections
Connect the AD911x-DPG2-EBZ board to the FMC Interposer board.
Connect the FMC Interposer board to the FMC-LPC connector of ML605 board.
Connect power cable to ML605.
Connect two
USB cables from the PC to the
JTAG and
UART USB connectors on ML605.
Turn on the ML605 Board
Connect a
USB cable to the AD911x-DPG2-EBZ board.
Programming the FPGA
Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set to 115200 baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../ad911x/sw/AD911x.bit).
Setting up uC/Probe
Launch Micrium uC/Probe and load the interface located in the project folder (../ad911x/sw/AD911x_Interface.wsp). In options, select RS-232 and set Baud Rate to 115200.
uC/Probe Interface
Click Play, and afterwards click on the ON/OFF Button. The Green LED on the button should light up. Set the options you desire by clicking on the red buttons and moving the sliders. After you are finished setting up the device, press “SEND AD911x SETTINGS” button. Now the device is programmed, and you should see the results on the S4 and S6 connectors on the AD911x Evaluation Board.
The User Interface is divided in 13 sections, described below:
Section 1 Communication with the board is activated / deactivated by toggling the ON/OFF Switch
Section 2 Modifies data format sent to the AD911x by toggling the switches ON or OFF:
Section 3 Modifies the way data is received from the DDS Module:
TWOS sets the input data format (ON = Twos complement, OFF = Unsigned Binary)
IFIRST selects pairing of input data (ON = I First on data input pads, OFF = Q First on data input pads)
IRISING selects data latch edge (ON = I data latched on rising edge, OFF = Q data latched on rising edge)
SIMUL selects DCLKIO type (ON = do not allow simultaneous input and output on DCLKIO, OFF = allow simultaneous input and output on DLCKIO)
Section 4 is used to select IRset and QRset Resistor values, using the corresponding slider
Section 5 selects differend Power Down possibilities:
LDOOFF sets the LDO Voltage regulator ON/OFF
LDOSTAT shows the status of LDO Voltage regulator
PWRDN Enables or Disables Power Supply (ON = Power Down, OFF = Power On)
ISLEEP turns I DAC output current ON/OFF
QSLEEP turns Q DAC output current ON/OFF
ICLKOFF turns I DAC Clock ON/OFF
QCLKOFF turns Q DAC Clock ON/OFF
EXTREF selects internal voltage reference (ON = Reference OFF, OFF = Reference ON)
Section 6
Section 7 is used to set the increment value for the DDS Core using the sliders provided
Section 8 Set different clock modes (see datasheet pg. 42 for details)
Section 9 Turn the Auxiliary DAC ON or OFF, set their Offset and Voltage Range
Section 10 provides calibration options for the AD911x
CALSELI selects calibration for I Channel
CALSELQ selects calibration for Q Channel
DIVSEL selects clock divide ratio by 2^n (n value selected using slider)
CALEN starts calibration process
CALSTATI shows the status of the calibration process for I Channel (Green = Done)
CALSTATQ shows the status of the calibration process for Q Channel (Green = Done)
Section 11 is used to set parameters for AD9512 Clock Distribution IC (divide ratio for Data and DAC Clock)
Section 12 User must press the button in order for the AD911x related modifications to take place
Section 13 User must press the button in order for the AD9512 related modifications to take place
If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again.
If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again.
In
Section 10 please select DIVSEL so that (DCLKIO / 2^n) is between 0.5
MHz and 4
MHz for optimal Calibration results
Downloads