Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (28 Sep 2012 11:31) was approved by AdrianC.The Previously approved version (28 May 2012 15:52) is available.Diff

This is an old revision of the document!


AD8403 FMC-SDP Interposer & Evaluation Board / Xilinx KC705 Reference Design

Supported Devices

Evaluation Boards

Overview

This document presents the steps to setup an environment for using the EVAL-AD8403SDZ evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the Micrium µC-Probe run-time monitoring tool. Below is presented a picture of the EVAL-AD8403SDZ Evaluation Board with the Xilinx KC705 board.

img_ad8403.jpg

For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to use the part evaluation setup. This consists of:

  • 1. A controller board like the SDP-B ( EVAL-SDP-CS1Z)
  • 2. The component SDP compatible product evaluation board
  • 3. Corresponding PC software ( shipped with the product evaluation board)

The SDP-B controller board is part of Analog Devices System Demonstration Platform (SDP). It provides a high speed USB 2.0 connection from the PC to the component evaluation board. The PC runs the evaluation software. Each evaluation board, which is an SDP compatible daughter board, includes the necessary installation file required for performance testing.

Note: it is expected that the analog performance on the two platforms may differ.

28 Sep 2012 10:32 · AdrianC

Below is presented a picture of SDP-B Controller Board with the EVAL-AD8403SDZ Evaluation Board.

The AD8403 is a quad-channel, 256-position, digitally controlled variable resistor device. This device performs the same electronic adjustment function as a mechanical potentiometer or variable resistor. The AD8403 contains four independent variable resistors. Each variable resistor offers a completely programmable value of resistance between the A terminal and the wiper or the B terminal and the wiper. The fixed A-to-B terminal resistance of 1 kO, 10 kO, 50 kO, or 100 kO has a ±1% channel-to-channel matching tolerance with a nominal temperature coefficient of 500 ppm/°C.

The EVAL-AD8403SDZ evaluation board is designed to help customers quickly prototype new AD8403 circuits and reduce design time. The EVAL-AD8403SDZ incorporates several test circuits to evaluate the AD8403 performance.

More information

Getting Started

The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project.

Required Hardware

Required Software

  • Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack).
  • uC-Probe run-time monitoring tool

Downloads

The following table presents a short description the reference design archive contents.

Folder Description
Bit Contains the KC705 configuration file that can be used to program the system for quick evaluation.
Microblaze Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA.
Software Contains the source files of the software project that will be run by the Microblaze processor.
uCProbeInterface Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microblaze memory.

Run the Demonstration Project

Hardware Setup

Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.

  • Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.
  • Connect the JTAG and UART cables to the KC705 and power up the FPGA board.
  • Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Kintex 7 device (see screenshot below).

  • Program the KC705 FPGA using the “Bit/download.bit” file provided in the reference design archive.
  • Power the ADI evaluation board.

At this point everything is set up and it is possible to start the evaluation of the ADI hardware through the controls in the uC-Probe application provided in the reference design.

Configure uC-Probe

Launch uC-Probe from the Start → All Programs → Micrium → uC-Probe.

Select uC-Probe options.

  • Click on the uC-Probe icon on the top left portion of the screen.
  • Click on the Options button to open the dialog box.

Set target board communication protocol as RS-232

  • Click on the Communication tab icon on the top left portion of the dialog box
  • Select the RS-232 option.

Setup RS-232 communication settings

  • Select the RS-232 option from the Communication tab.
  • Select the COM port to which the KC705 board is connected.
  • Set the Baud Rate to 115200 bps.

  • Press Apply and OK to exit the options menu.

Load and Run the Demonstration Project

  • Click the Open option from the uC-Probe menu and select the .wsp file from the ucProbeInterface folder provided within the reference design files.
  • Before opening the interface uC-Probe will ask for a symbols file that must be associated with the interface. Select the file ucProbeInterface/ADIEvalBoard.elf to be loaded as a symbol file.
  • Run the demonstration project by pressing the Play button.

  • In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the Stop button and run it again by pressing the Play button.
  • After starting the uC-Probe interface wait until the status of the connection with the board displayed on the bottom of the screen is set to Connected. It is possible to use the interface only after the status is changed to Connected and the data transfer speed displayed next to the connection status is different than 0.
16 Feb 2012 09:23 · acozma

Demonstration Project User Interface

The following figure presents the uC-Probe interface that can be used for monitoring and controlling the operation of the EVAL-AD8403SDZ evaluation board.

Section A is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the ON/OFF switch. The Activity LED turns green when the communication is active. If the ON/OFF switch is set to ON and the Activity LED is BLACK it means that there is a communication problem with the board.

Section B is used to shutdown and reset the device.

  • Shutdown: When it is pressed, forces the resistors to an end-to-end open-circuit condition on the A terminal and shorts the wiper to the B terminal, achieving a microwatt power shutdown state. When it is released, the previous latch settings put the wiper in the same resistance setting prior to shutdown.
  • Reset: When it is pressed, forces the wiper to midscale by loading 80H into the VR latch. When it is released, the VR latch remains loaded with 80H, but you can load the desired values.

Section C is used to send a 10-bits word to the device. This data-word can be sent by manually switching the buttons from 0 to 1 or from 1 to 0, as desired, and then toggling the Send Data switch.

Section D is used to update the RDAC registers by selecting a desirable value on the slider and toggling the Load RDACx switch.

Troubleshooting

In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues:

  • Check that the evaluation board is powered as instructed in the board's user guide.
  • In uC-Probe refresh the symbols file by right-clicking on the System Browser window and selecting Refresh Symbols.
  • If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again.

More information

28 May 2012 15:18
resources/fpga/xilinx/interposer/ad8403.1348824702.txt.gz · Last modified: 28 Sep 2012 11:31 by AdrianC