This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad7988-5 [28 May 2012 15:41] – Approved Alexandru.Tofan | resources:fpga:xilinx:interposer:ad7988-5 [14 Jan 2021 06:09] (current) – use xilinx> interwiki links Robin Getz | ||
---|---|---|---|
Line 16: | Line 16: | ||
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7988-5SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7988-5SDZ** Evaluation Board. | ||
Line 32: | Line 28: | ||
* [[adi> | * [[adi> | ||
* {{: | * {{: | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 40: | Line 36: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD7988-5SDZ** evaluation board | * **EVAL-AD7988-5SDZ** evaluation board | ||
Line 66: | Line 62: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 80: | Line 76: | ||
{{ : | {{ : | ||
- | <note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | + | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |