This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad7988-5 [22 Mar 2012 08:05] – [Overview] Andrei Cozma | resources:fpga:xilinx:interposer:ad7988-5 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 16: | Line 16: | ||
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * a compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7988-5SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7988-5SDZ** Evaluation Board. | ||
Line 66: | Line 62: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 80: | Line 76: | ||
{{ : | {{ : | ||
- | <note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | + | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' |
====== More information ====== | ====== More information ====== | ||
- | * [[ez>community/ | + | {{page>ez_common}} |