resources:fpga:xilinx:interposer:ad7983 [28 Sep 2012 10:41]
Adrian Costina Added common section for describing the evaluation setup and System Demonstration Platform
resources:fpga:xilinx:interposer:ad7983 [14 Jan 2021 06:09] (current)
Robin Getz use xilinx> interwiki links
Line 29: Line 29:
   * [[adi>​AD7983|AD7983 Product Info]] - pricing, samples, datasheet   * [[adi>​AD7983|AD7983 Product Info]] - pricing, samples, datasheet
   * {{:​resources:​fpga:​altera:​bemicro:​user_guide_eval_10lead_pulsar.pdf|EVAL-AD7980SDZ evaluation board user guide}}   * {{:​resources:​fpga:​altera:​bemicro:​user_guide_eval_10lead_pulsar.pdf|EVAL-AD7980SDZ evaluation board user guide}}
-  * [[http://www.xilinx.com/products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]+  * [[xilinx>products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 37: Line 37:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * [[http://www.xilinx.com/products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]+  * [[xilinx>products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
   * FMC-SDP adapter board   * FMC-SDP adapter board
   * **EVAL-AD7983SDZ** evaluation board   * **EVAL-AD7983SDZ** evaluation board
Line 63: Line 63:
 ===== Hardware Setup ===== ===== Hardware Setup =====
  
-<note important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</note>+<WRAP important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</WRAP>
  
   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.
Line 77: Line 77:
 {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_adc.png?​400 }} {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_adc.png?​400 }}
  
-<note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn'​t appear anymore.</​note>+<WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn'​t appear anymore.</​WRAP>
  
 ====== More information ====== ====== More information ======
 {{page>​ez_common}} {{page>​ez_common}}
resources/fpga/xilinx/interposer/ad7983.1348821702.txt.gz · Last modified: 28 Sep 2012 10:41 by Adrian Costina