Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad7690 [28 May 2012 15:40]
Alexandru.Tofan Approved
resources:fpga:xilinx:interposer:ad7690 [14 Jan 2021 06:09] (current)
Robin Getz use xilinx> interwiki links
Line 16: Line 16:
 {{ :​resources:​fpga:​xilinx:​interposer:​ad7980.jpg?​400 }} {{ :​resources:​fpga:​xilinx:​interposer:​ad7980.jpg?​400 }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping,​ the user is directed to Analog Devices [[/​resources/​eval/​sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/​eval/​sdp/​sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * a compatible Analog Devices SDP [[adi>sdp#​exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. ​ Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7690SDZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7690SDZ** Evaluation Board.
Line 33: Line 29:
   * [[adi>​AD7690|AD7690 Product Info]] - pricing, samples, datasheet   * [[adi>​AD7690|AD7690 Product Info]] - pricing, samples, datasheet
   * {{:​resources:​fpga:​altera:​bemicro:​user_guide_eval_10lead_pulsar.pdf|EVAL-AD7690SDZ evaluation board user guide}}   * {{:​resources:​fpga:​altera:​bemicro:​user_guide_eval_10lead_pulsar.pdf|EVAL-AD7690SDZ evaluation board user guide}}
-  * [[http://www.xilinx.com/products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]+  * [[xilinx>products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 41: Line 37:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * [[http://www.xilinx.com/products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]+  * [[xilinx>products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
   * FMC-SDP adapter board   * FMC-SDP adapter board
   * **EVAL-AD7690SDZ** evaluation board   * **EVAL-AD7690SDZ** evaluation board
Line 67: Line 63:
 ===== Hardware Setup ===== ===== Hardware Setup =====
  
-<note important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</note>+<WRAP important>​Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</WRAP>
  
   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.
Line 81: Line 77:
 {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_adc.png?​400 }} {{ :​resources:​fpga:​xilinx:​interposer:​teraterm_adc.png?​400 }}
  
-<note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn'​t appear anymore.</​note>+<WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn'​t appear anymore.</​WRAP>
  
 ====== More information ====== ====== More information ======
 {{page>​ez_common}} {{page>​ez_common}}
resources/fpga/xilinx/interposer/ad7690.1338212412.txt.gz · Last modified: 28 May 2012 15:40 by Alexandru.Tofan