This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:fpga:xilinx:interposer:ad7686 [08 Oct 2012 17:05] – created Alexandru.Tofan | resources:fpga:xilinx:interposer:ad7686 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 64: | Line 64: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | <note important> | + | <WRAP important> |
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
Line 78: | Line 78: | ||
{{ : | {{ : | ||
- | <note tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | + | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |