This shows you the differences between two versions of the page.
Last revision | |||
— | resources:fpga:xilinx:interposer:ad7366 [25 Feb 2013 13:46] – created Adrian Costina | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== AD7366 FMC-SDP Interposer & Evaluation Board / Xilinx KC705 Reference Design ====== | ||
+ | |||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ====== Overview ====== | ||
+ | |||
+ | This document presents the steps to setup an environment for using the **[[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7366SDZ** Evaluation Board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The **EVAL-AD7366SDZ** evaluation board is a member of a growing number of boards available for the **SDP**. It was designed to help customers evaluate performance or quickly prototype new **AD7366** circuits and reduce design time. | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | ===== More information ===== | ||
+ | * [[adi> | ||
+ | * EVAL-AD7366SDZ evaluation board user guide is included on the CD as part of the Evaluation Board Kit | ||
+ | * [[http:// | ||
+ | |||
+ | ====== Getting Started ====== | ||
+ | |||
+ | The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project. | ||
+ | |||
+ | ===== Required Hardware ===== | ||
+ | |||
+ | * [[http:// | ||
+ | * FMC-SDP adapter board | ||
+ | * **EVAL-AD7366SDZ** evaluation board | ||
+ | |||
+ | ===== Required Software ===== | ||
+ | |||
+ | * Xilinx ISE 14.4 | ||
+ | * A UART terminal (ex. TeraTerm / Hyperterminal). | ||
+ | |||
+ | ===== Downloads ===== | ||
+ | |||
+ | * {{: | ||
+ | |||
+ | The following table presents a short description the reference design archive contents. | ||
+ | |||
+ | ^ **Folder** ^ **Description** ^ | ||
+ | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | ||
+ | | DataCapture | Contains the script used to read data from the ADC and save it into a file on the PC. | | ||
+ | | Hdl | Contains the HDL driver for the AD7366 ADC. | | ||
+ | | Microblaze | Contains the EDK 14.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | ||
+ | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | ||
+ | |||
+ | ====== Run the Demonstration Project ====== | ||
+ | |||
+ | ===== Hardware Setup ===== | ||
+ | |||
+ | <WRAP important> | ||
+ | |||
+ | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
+ | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
+ | * Start IMPACT, and double click “// | ||
+ | {{ : | ||
+ | * Program the KC705 FPGA using the "// | ||
+ | * Power the ADI evaluation board. | ||
+ | * Start a UART terminal and set the baud rate to 115200 bps. | ||
+ | |||
+ | At this point everything is set up and it is possible to start the evaluation of the ADI hardware. To capture data from the ADC run the // | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP tip>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> | ||