Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:xilinx:interposer:ad7291 [28 May 2012 15:28]
Alexandru.Tofan Approved
resources:fpga:xilinx:interposer:ad7291 [28 Sep 2012 10:35] (current)
AdrianC Added common section for describing the evaluation setup and System Demonstration Platform
Line 15: Line 15:
 {{ :​resources:​fpga:​xilinx:​interposer:​ad7291.jpg?​400 }} {{ :​resources:​fpga:​xilinx:​interposer:​ad7291.jpg?​400 }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping,​ the user is directed to Analog Devices [[/​resources/​eval/​sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/​eval/​sdp/​sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * a compatible Analog Devices SDP [[adi>sdp#​exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. ​ Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7291SDZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7291SDZ** Evaluation Board.
resources/fpga/xilinx/interposer/ad7291.txt · Last modified: 28 Sep 2012 10:35 by AdrianC