This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:xilinx:interposer:ad7091 [10 Feb 2021 10:33] – [Downloads] Fix broken link Istvan Csomortani | resources:fpga:xilinx:interposer:ad7091 [11 Feb 2021 08:35] (current) – Fix broken link Istvan Csomortani | ||
---|---|---|---|
Line 91: | Line 91: | ||
* All these files must be copied into the **%Working directory%/ | * All these files must be copied into the **%Working directory%/ | ||
* The SDK should automatically build the project and the Console window will display the result of the build. If the build is not done automatically, | * The SDK should automatically build the project and the Console window will display the result of the build. If the build is not done automatically, | ||
- | * If the project was built without any errors, you need to download the data capture script, from [[https:// | + | * If the project was built without any errors, you need to download the data capture script, from [[https:// |
* Run the **data_capture.bat** script. If the acquisition is finished with success, it should appear a file called **Acquisition.csv** with the result of the conversion. | * Run the **data_capture.bat** script. If the acquisition is finished with success, it should appear a file called **Acquisition.csv** with the result of the conversion. | ||
{{: | {{: |