Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:xilinx:interposer:ad5790 [28 Sep 2012 11:25]
AdrianC Added common section for describing the evaluation setup and System Demonstration Platform
resources:fpga:xilinx:interposer:ad5790 [30 Sep 2013 15:25] (current)
LucianS changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact
Line 11: Line 11:
 ====== Overview ====== ====== Overview ======
  
-This document presents the steps to setup an environment for using the **[[adi>​AD5790|EVAL-AD5790SDZ]]** evaluation board together with the Xilinx KC705 FPGA boardthe Xilinx Embedded Development Kit (EDK) and the [[http://​micrium.com/​page/​products/​tools/​probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5790SDZ Evaluation Board with the Xilinx KC705 board.+This document presents the steps to setup an environment for using the **[[adi>​AD5790|EVAL-AD5790SDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). ​ Below is presented a picture of the EVAL-AD5790SDZ Evaluation Board with the Xilinx KC705 board.
  
 {{ :​resources:​fpga:​xilinx:​interposer:​img_ad5790.jpg?​400 }} {{ :​resources:​fpga:​xilinx:​interposer:​img_ad5790.jpg?​400 }}
Line 29: Line 29:
   * [[adi>/​static/​imported-files/​user_guides/​UG-342.pdf|EVAL-AD5790SDZ evaluation board user guide]]   * [[adi>/​static/​imported-files/​user_guides/​UG-342.pdf|EVAL-AD5790SDZ evaluation board user guide]]
   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
-  * [[http://​micrium.com/​page/​products/​tools/​probe|Micrium uC-Probe]] 
  
 ====== Getting Started ====== ====== Getting Started ======
Line 43: Line 42:
 ===== Required Software ===== ===== Required Software =====
  
-  * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack)+  * Xilinx ISE 14.6
-  * [[http://micrium.com/​page/​products/​tools/​probe|uC-Probe]] run-time monitoring tool+  * UART Terminal (Termite/Tera Term/Hyperterminal),​ baud rate 115200. 
 +  * The EVAL-AD5790 reference project for Xilinx KC705 FPGA.
  
 ===== Downloads ===== ===== Downloads =====
- +<WRAP round download 80%> 
-  * {{:resources:​fpga:xilinx:​interposer:​ad5790_evalboard.zip|Reference Design Files}} +\\ 
- +  * **AD5790 Driver:** https://github.com/​analogdevicesinc/​no-OS/​tree/​master/​device_drivers/​AD5791 
-The following table presents a short description the reference design archive contents. +  * **AD5790 Commands:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​device_commands/​AD5791 
- +  ​* **Xilinx Boards Common Drivers:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​platform_drivers/​Xilinx/​SDP_Common 
-**Folder** **Description** +  * **EDK KC705 Reference ​project:** https://​github.com/​analogdevicesinc/​fpgahdl_xilinx/​tree/​master/​cf_sdp_kc705 
-| Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation| +\\ 
-| Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | +</​WRAP>​
-| Software | Contains the source files of the software ​project ​that will be run by the Microblaze processor.| +
-| uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. |+
  
 ====== Run the Demonstration Project ====== ====== Run the Demonstration Project ======
  
-{{page>​ucprobe_common}} +===== Hardware setup =====
- +
-===== Demonstration Project User Interface ​===== +
- +
-The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5790SDZ** evaluation board. +
- +
-{{ :​resources:​fpga:​altera:​bemicro:​ad5790interface.png?​700 }} +
- +
-The communication with the board is activated / deactivated by toggling the **//​ON/​OFF//​** switch. The **//​Activity//​** LED turns green when the communication is active. If the **//​ON/​OFF//​** switch is set to **//ON//** and the Activity LED is BLACK it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. +
- +
-The value of the AD5790 //DAC Register// is changed using the slider located under the **//DAC Register Value (20-bit)//​** label. The selected value is displayed in the numeric box located next to the slider. Next to it, the value that is read from the DAC register is displayed. The slider will select the DAC value as a binery offset value. In case the coding on the DAC is 2's Complement, the value set and the readback value will differ.+
  
-The value of the AD5790 Clearcode Register is changed using the slider located under the **//​Clearcode Register Value (20-bit)//​** label. The selected value is displayed in the numeric box located next to the sliderNext to it, the value that is read from the Clearcode register is displayed.+<WRAP round important 80%> 
 +\\ 
 +Before connecting ​the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change ​the setting for VADJ_FPGA visit the Xilinx KC705 product page. 
 +</​WRAP>​
  
-The sliders ​**//​Vref+//​** and **//Vref-//** are used to specify the reference voltages set on the evaluation board. ​The default values are +10V and -10V.+  ​Use the FMC-SDP interposer ​to connect ​the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. 
 +  * Connect the JTAG and UART cables to the KC705 and power up the FPGA board.
  
-The DAC’s output voltage is displayed in the numeric box having the label **//Output voltage//**This value is computed based on the Vref+ and Vref- values.+<WRAP round important 80%> 
 +\\ 
 +To power on the EVAL-AD5790 evaluation board, you need to provide external differential supply voltage to J2 connector(for more information see: [[adi>/static/imported-files/user_guides/UG-342.pdf|EVAL-AD5790SDZ evaluation board user guide]]) and a 5V reference voltage to VREF connector ​on the evaluation boardVREFN will be connected to AGND (LK8 option=B, LK2 option=B, LK3 option=B, LK4 inserted). 
 +</​WRAP>​
  
-The values of the //Control Register’s//​ bits are indicated by the LEDs situated under the **//Control Register//​** label. When a LED id lit it means that the corresponding bit’s value is 1. Each switch under the LEDs can be used to toggle the corresponding bit in the Control register. 
  
-The values ​of the //Software Control Register’s// bits are indicated by the LEDs situated under the **//Status Control Register//** labelWhen a LED is lit it means that the corresponding ​bit’s value is 1. Each switch can be used to toggle ​the corresponding ​bit in the Software Control Register.+===== Reference Project Overview ===== 
 +The following commands were implemented in this version ​of EVAL-AD5790 reference project for Xilinx KC705 FPGA board. 
 +^ Command ^ Description ^ 
 +| **help?** | Displays all available commands. | 
 +| **reset!** | Resets ​the device. | 
 +| **coding=** | Selects the coding style. Accepted values:\\ 0 - Two'complement coding.(default)\\ 1 - Offset binary coding. | 
 +| **coding?** | Display ​the current coding style. | 
 +| **register=** | Writes to the DAC register. Accepted values:\\ 0 .. 1048575 - the value written to the DAC. | 
 +**register?** | Displays last written value to the DAC register
 +| **voltage=** | Sets the DAC output voltage. Accepted values:\\ -10 .. +10 - desired output voltage in volts. | 
 +| **voltage?​** | Displays the output voltage. | 
 +| **output=** | Selects the DAC output state. Accepted values:\\ 0 - Normal state.\\ 1 - Clamped via 6KOhm to AGND.(default)\\ 2 - Tristate. | 
 +| **output?** | Displays the DAC output state. | 
 +| **rbuf=** | Sets/resets the RBUF bit from control register. Accepted values:\\ 0 - RBUF is reset.\\ ​- RBUF is set.(default) | 
 +| **rbuf?** | Displays ​the value of RBUF bit from control register|
  
-The hardware pins can be controlled by the switches under the label "​Hardware pins". When the switch is active, the corresponding pin will be activated (will be toggled LOW). 
  
 +Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
  
-===== Troubleshooting =====+The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. 
 +{{ :​resources:​fpga:​xilinx:​interposer:​Terminal_KC705.jpg?​ }}
  
-In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: +===== Software Project Setup ===== 
-  * Check that the evaluation board is powered as instructed in the board'​s user guide. +{{page>​import_workspace}}
-  * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//​**. +
-  * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again.+
  
 ====== More information ====== ====== More information ======
   * [[resources:​tools-software:​linux-drivers:​iio-dac:​ad5791|AD5790 IIO DAC Linux Driver]]   * [[resources:​tools-software:​linux-drivers:​iio-dac:​ad5791|AD5790 IIO DAC Linux Driver]]
 {{page>​ez_common}} {{page>​ez_common}}
resources/fpga/xilinx/interposer/ad5790.txt · Last modified: 30 Sep 2013 15:25 by LucianS