Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad5755 [06 Apr 2012 15:35]
ACozma [More information]
resources:fpga:xilinx:interposer:ad5755 [22 Jul 2019 13:44] (current)
AndreiD1994 Update no-OS driver link
Line 14: Line 14:
 ====== Overview ====== ====== Overview ======
  
-This document presents the steps to setup an environment for using the **[[adi>​AD5755|EVAL-AD5755SDZ]]** evaluation board together with the Xilinx KC705 FPGA boardthe Xilinx Embedded Development Kit (EDK) and the [[http://​micrium.com/​page/​products/​tools/​probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5755SDZ Evaluation Board with the Xilinx KC705 board.+This document presents the steps to setup an environment for using the **[[adi>​AD5755|EVAL-AD5755SDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5755SDZ Evaluation Board with the Xilinx KC705 board.
  
 {{ :​resources:​fpga:​xilinx:​interposer:​img_ad5755.jpg }} {{ :​resources:​fpga:​xilinx:​interposer:​img_ad5755.jpg }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping,​ the user is directed to Analog Devices [[/​resources/​eval/​sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/​eval/​sdp/​sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * a compatible Analog Devices SDP [[adi>sdp#​exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. ​ Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5755SDZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5755SDZ** Evaluation Board.
Line 36: Line 32:
   * [[adi>/​static/​imported-files/​user_guides/​UG-244.pdf|EVAL-AD5755SDZ evaluation board user guide]]   * [[adi>/​static/​imported-files/​user_guides/​UG-244.pdf|EVAL-AD5755SDZ evaluation board user guide]]
   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]   * [[http://​www.xilinx.com/​products/​boards-and-kits/​EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
-  * [[http://​micrium.com/​page/​products/​tools/​probe|Micrium uC-Probe]] 
  
 ====== Getting Started ====== ====== Getting Started ======
Line 50: Line 45:
 ===== Required Software ===== ===== Required Software =====
  
-  * Xilinx ISE 13.(Programmer (IMPACT) is sufficient for the demo and is available on Webpack). +  * Xilinx ISE 14.(Programmer (IMPACT) is sufficient for the demo and is available on Webpack). 
-  * [[http://​micrium.com/​page/​products/​tools/​probe|uC-Probe]] run-time monitoring tool+  * UART Terminal (Tera Term/Hyperterminal),​ baud rate 115200
  
 ===== Downloads ===== ===== Downloads =====
 +<WRAP round download 80%>
 +\\
 +  * **AD5755 Driver:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​drivers/​dac/​ad5755
 +  * **AD5755 Commands:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​device_commands/​AD5755
 +  * **Xilinx Boards Common Drivers:** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​platform_drivers/​Xilinx/​SDP_Common
 +  * **EDK KC705 Reference project:** https://​github.com/​analogdevicesinc/​fpgahdl_xilinx/​tree/​master/​cf_sdp_kc705
 +\\
 +</​WRAP>​
  
-  * {{:​resources:​fpga:​xilinx:​interposer:​ad5755_evalboard.zip|Reference Design Files}}+===== Hardware setup =====
  
-The following table presents a short description ​the reference design archive contents.+<WRAP round important 80%> 
 +\\ 
 +Before connecting ​the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. 
 +</​WRAP>​
  
-**Folder** ^ **Description** ^ +  ​Use the FMC-SDP interposer ​to connect ​the ADI evaluation ​board to the Xilinx ​KC705 board on the FMC LPC connector
-| Bit | Contains ​the KC705 configuration file that can be used to program ​the system for quick evaluation. | +  * Connect ​the JTAG and UART cables ​to the KC705 and power up the FPGA board.
-| Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | +
-| Software | Contains the source files of the software project that will be run by the Microblaze processor.| +
-| uCProbeInterface | Contains ​the uCProbe interface ​and the .elf symbols file used by uC-Probe ​to access data from the Microblaze memory|+
  
-====== Run the Demonstration Project ======+<WRAP round important 80%> 
 +\\ 
 +To power on the EVAL-AD5755 evaluation board, you need to provide an external +15V AVdd and -15V AVss analog supply voltage and a +5V AVcc DC-to-DC supply voltage, which will supplies all four on-board dc-to-dc blocks and may draw as much as 0.8 A peak current per channel (for more information see: [[adi>/​static/​imported-files/​user_guides/​UG-244.pdf|EVAL-AD5755SDZ evaluation board user guide]]). 
 +</​WRAP>​
  
-{{page>​ucprobe_common}}+===== Reference Project Overview ===== 
 +The following commands were implemented in this version of EVAL-AD5755 reference project for Xilinx KC705 FPGA board. 
 +^ Command ^ Description ^ 
 +| **help?** | Displays all available commands. | 
 +| **register=** | Writes to the a data register. Accepted values:\\ **Register address:​**\\ 0 - DAC Data Reg \\ 2 - Gain Register \\ 3 - Gain Register All DACs \\ 4 - Offset Register \\ 5 - Offset Register All DACs \\ 6 - Clear Code Register \\ 7 - Control Register \\ **Channel:​**\\ 0 .. 3 - channel A .. D. \\ **Value:​**\\ 0 .. 65535 - the value written to the DAC.\\ | 
 +| **control=** | Writes to the a control register. Accepted values:\\ **Register address:​**\\ 0 - Slew Rate Register \\ 1 - Main Control Register \\ 2 - DAC Control Register \\ 3 - Dc-to-dc Control Register \\ 4 - Software Register \\ **Channel:​**\\ 0 .. 3 - channel A .. D. \\ **Value:​**\\ 0 .. 65535 - the value written to the DAC.\\ | 
 +| **register?​** | Read back the value of a specified register. Accepted values:\\ Register address : 0x00 .. 0x1A. | 
 +| **power=** | Set the power state of the dc-to-dc converters, DAC and internal amplifiers for the selected channel. Accepted values:\\ **Channel:​**\\ 0 .. 3 - channel A .. D.\\ **Value:​**\\ 0 - turn off; 1 - turn on. | 
 +| **power?** | Displays the power state of the dc-to-dc converters,​DAC and internal amplifiers for the selected channel. Accepted values:\\ **Channel:​**\\ 0 .. 3 - channel A .. D. | 
 +| **range=** | Set the range of the selected channel. Accepted values:\\ **Channel:​**\\ 0 .. 3 - channel A .. D.\\ **Range:​**\\ ​ 0 - 0 V to 5 V voltage\\ 1 - 0 V to 10 V voltage\\ 2 - -5 V to +5 V voltage\\ 3 - -10 V to +10 V voltage\\ 4 - 4 mA to 20 mA current\\ 5 - 0 mA to 20 mA current\\ 6 - 0 mA to 24 mA current| 
 +| **range?** | Displays the range of the selected channel. Accepted values: \\ **Channel:​**\\ 0 .. 3 - channel A .. D.| 
 +| **voltage=** | Sets the output voltage for a selected channel. Accepted values: \\ **Channel:​**\\ 0 .. 3 - channel A .. D.\\ Desired voltage(unit in V) multiplied by 1000 | 
 +| **voltage?​** | Displays the output voltage for a selected channel. Accepted values:\\ **Channel:​**\\ 0 .. 3 - channel A .. D.| 
 +| **current=** | Displays the output current for a selected channel. Accepted values: \\ **Channel:​**\\ 0 .. 3 - channel A .. D.\\ Desired current (unit in mA) multiplied by 1000 | 
 +| **current?​** | Displays the output current for a selected channel. Accepted values: \\ **Channel:​**\\ 0 .. 3 - channel A .. D. | 
 +| **getStatus!** | Read back the Status register and print any faults or errors. | 
 +| **testSPI!** | Ensure that the SPI interface are working correctly. | 
 +  
 +Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
  
-===== Demonstration Project User Interface =====+The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. 
 +{{ :​resources:​fpga:​xilinx:​interposer:​Terminal_KC705.jpg?​ }}
  
-The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5755SDZ** evaluation board. +===== Software Project Setup ===== 
- +{{page>​import_workspace}}
-{{ :​resources:​fpga:​altera:​bemicro:​ad5755_interface.png?​700 }} +
- +
-**Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the **//​ON/​OFF//​** switch. The **//​Activity//​** LED turns green when the communication is active. If the **//​ON/​OFF//​** switch is set to **//ON//** and the **//​Activity//​** LED is **//​BLACK//​** it means that there is a communication problem with the board. +
- +
-**Section B** is used to select the DAC channel. +
- +
-**Section C** is used to write data into the register selected by the Selection Slider. +
- +
-Options: +
- +
-  * Write to DAC data register (individual channel write). +
-  * Write to gain register (individual channel write). +
-  * Write to gain register (all DACs). +
-  * Write to offset register (individual channel write). +
-  * Write to offset register (all DACs) . +
-  * Write to clear code register (individual channel write). +
- +
-**Section D** is used to read data from the register selected by the Selection Slider. +
- +
-Options: +
- +
-  * Read from DAC data register (individual channel read). +
-  * Read from DAC control register (individual channel read). +
-  * Read from Gain register (individual channel read). +
-  * Read from Offset register (individual channel read). +
-  * Read from Clear Code register (individual channel read). +
-  * Read from Slew Rate control register (individual channel read). +
-  * Read from Status register. +
-  * Read from Main control register. +
-  * Read from DC-to-DC control register. +
- +
-**Section E** is used to write data into the DAC n Control Register. +
- +
-Options: +
- +
-  * Internal – Powers up the dc-to-dc converter, DAC, and internal amplifiers for the selected channel. +
-  * Clear – Clear enable bit. +
-  * Output – Enables/​disables the selected output channel. +
-  * Rset – Selects an internal or external current sense resistor for the selected DAC channel. +
-  * DC-DC – Powers the dc-to-dc converter on the selected channel. +
-  * OVRNG – Enables 20% overrange on voltage output channel only. No current output overrange available. +
-  * Output Range – Selects the output range to be enabled. +
- +
-**Section F** is used to write data into the DC-DC Control Register. +
- +
-Options: +
- +
-  * DC-DC Comp – Selects between an internal and external compensation resistor for the dc-to-dc converter. +
-  * Phase – User programmable dc-to-dc converter phase (between channels). +
-  * Frequency – DC-to-dc switching frequency. +
-  * Max Voltage – Maximum allowed VBOOST_x voltage supplied by the dc-to-dc converter. +
- +
-**Section G** is used to write data into the Main Control Register. +
- +
-Options: +
- +
-  * POC – The POC bit determines the state of the voltage output channels during normal operation. +
-  * StartRead – Enable status readback during a write. +
-  * EWD – Enable watchdog timer. +
-  * WD Period – Select the timeout period for the watchdog timer. +
-  * ShtCctLim – Programmable short-circuit limit on the VOUT_x pin in the event of a short-circuit condition. +
-  * OutEn All – Enables the output on all four DACs simultaneously. +
-  * DC-DC All – Powers up the dc-to-dc converter on all four channels simultaneously. +
- +
-**Section H** is used to write data into the Slew Rate Control Register. +
- +
-Options: +
- +
-  * SE – Enable SE. +
-  * SR Clock – Slew Rate Update Clock Options. +
-  * SR Step – Slew Rate Step Size Options. +
- +
-**Section I** is used to write data into the Software Register. +
- +
-Options: +
- +
-  * User Bit – This bit is mapped to Bit D11 of the status register. +
-  * Software Reset – Performs a reset of the AD5755. +
- +
-===== Troubleshooting ​===== +
- +
-In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: +
-  * Check that the evaluation board is powered as instructed in the board'​s user guide. +
-  * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//​**. +
-  * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again.+
  
 ====== More information ====== ====== More information ======
   * [[resources:​tools-software:​linux-drivers:​iio-dac:​ad5755|AD5755 IIO DAC Linux Driver]]   * [[resources:​tools-software:​linux-drivers:​iio-dac:​ad5755|AD5755 IIO DAC Linux Driver]]
-  * [[ez>community/​fpga|ask questions about the FPGA reference design]]+{{page>ez_common}}
resources/fpga/xilinx/interposer/ad5755.1333719342.txt.gz · Last modified: 06 Apr 2012 15:35 by ACozma