This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad5694r [28 May 2012 15:44] Alexandru.Tofan Approved |
resources:fpga:xilinx:interposer:ad5694r [09 Jan 2021 00:48] (current) Robin Getz user interwiki links |
||
---|---|---|---|
Line 12: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board. | + | This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board. |
{{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }} | {{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }} | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices [[/resources/eval/sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/eval/sdp/sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** | + | |
- | * a compatible Analog Devices SDP [[adi>sdp#exallist|product evaluation board]] | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5694RSDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5694RSDZ** Evaluation Board. | ||
Line 33: | Line 29: | ||
* [[adi>AD5694R|AD5694R Product Info]] - pricing, samples, datasheet | * [[adi>AD5694R|AD5694R Product Info]] - pricing, samples, datasheet | ||
* EVAL-AD5694RSDZ evaluation board user guide | * EVAL-AD5694RSDZ evaluation board user guide | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | + | * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] |
- | * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]] | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 42: | Line 37: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | + | * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD5694R** evaluation board | * **EVAL-AD5694R** evaluation board | ||
Line 48: | Line 43: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool | + | * UART Terminal (Termite/Tera Term/Hyperterminal), baud rate 115200. |
+ | * The EVAL-AD5694R reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{:resources:fpga:xilinx:interposer:ad5694r_evalboard.zip|Reference Design Files}} | + | \\ |
- | + | * **AD5694R Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5686 | |
- | The following table presents a short description the reference design archive contents. | + | * **AD5694R Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5686 |
- | + | * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common | |
- | ^ **Folder** ^ **Description** ^ | + | * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705 |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </WRAP> |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | ===== Hardware Setup ===== | + | ===== Hardware setup ===== |
- | <note important>Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</note> | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </WRAP> | ||
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
* Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | * Start IMPACT, and double click “//Boundary Scan//”. Right click and select //Initialize Chain//. The program should recognize the Kintex 7 device (see screenshot below). | ||
- | {{ :resources:fpga:xilinx:interposer:impact_config.png?300 }} | ||
- | * Program the KC705 FPGA using the "//Bit/download.bit//" file provided in the reference design archive. | ||
- | * Power the ADI evaluation board. | ||
- | |||
- | At this point everything is set up and it is possible to start the evaluation of the ADI hardware through the controls in the uC-Probe application provided in the reference design. | ||
- | |||
- | ===== Configure uC-Probe ===== | ||
- | |||
- | Launch **uC-Probe** from the **//Start -> All Programs -> Micrium -> uC-Probe//**. | ||
- | |||
- | Select **uC-Probe** options. | ||
- | * Click on the **uC-Probe** icon on the top left portion of the screen. | ||
- | * Click on the **//Options//** button to open the dialog box. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:ucprobeoptionsbtn.png?300 }} | ||
- | |||
- | Set target board communication protocol as **//RS-232//** | ||
- | * Click on the **//Communication//** tab icon on the top left portion of the dialog box | ||
- | * Select the **//RS-232//** option. | ||
- | |||
- | {{ :resources:fpga:xilinx:interposer:ucprobe_comm.png?300 }} | ||
- | |||
- | Setup **//RS-232//** communication settings | ||
- | * Select the **//RS-232//** option from the **//Communication//** tab. | ||
- | * Select the COM port to which the KC705 board is connected. | ||
- | * Set the Baud Rate to 115200 bps. | ||
- | |||
- | {{ :resources:fpga:xilinx:interposer:ucprobe_rs232.png?300 }} | ||
- | |||
- | * Press **//Apply//** and **//OK//** to exit the options menu. | ||
- | |||
- | ===== Load and Run the Demonstration Project ===== | ||
- | |||
- | * Click the **//Open//** option from the **uC-Probe** menu and select the file **//ucProbeInterface/AD5694R_Interface.wsp//** provided within the reference design files. | ||
- | |||
- | * Before opening the interface **uC-Probe** will ask for a symbols file that must be associated with the interface. Select the file **//ucProbeInterface/ADIEvalBoard.elf//** to be loaded as a symbol file. | ||
- | |||
- | * Run the demonstration project by pressing the **//Play//** button. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:image081.png?200 }} | ||
- | |||
- | <note tip>In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **//Stop//** button and run it again by pressing the **//Play//** button.</note> | ||
- | |||
- | ===== Demonstration Project User Interface ===== | ||
- | |||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5694RSDZ** evaluation board. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:ad5694r_interface.png?700 }} | ||
- | |||
- | **Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the //ON/OFF// switch. The //Activity// LED turns green when the communication is active. If the //ON/OFF// switch is set to //ON// and the //Activity// LED is //BLACK// it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. | ||
- | |||
- | **Section B** is used to select the //Command// to be sent to the DAC. The definition of each command is available in Table 7 of the part's datasheet. | ||
- | |||
- | **Section C** is used to select the //Address// of the registers to be affected by the command, if the command is 1, 2 or 3. If the selected command is 5, the //Address// buttons will be used to program the //LDAK MASK REGISTER// for the corresponding DAC. For the other commands, they are ignored. | ||
- | |||
- | **Section D** is used to program the value to be written to the DAC registers. | ||
- | |||
- | **Section E** is used to send the selected command to the DAC. | ||
- | **Section F** is used to configure the databits sent for the command 4. Each DAC's power operation can be configured independently. | + | <WRAP round important 80%> |
+ | \\ | ||
+ | To power on the EVAL-AD5694R evaluation board, you need to apply +6V supply voltage to J3 connector of the board. | ||
+ | </WRAP> | ||
- | **Section G** is used to configure the databits sent for the command 7. If the button is pressed, the Internal reference will be turned off. | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-AD5694R reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **reset!** | Activate a power-on reset. | | ||
+ | | **load=** | Loads selected DAC input register with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
+ | | **update=** | Update the selected DAC channel with the input register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels. | | ||
+ | | **loadAndUpdate=** | Loads and updates the selected DAC with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
+ | | **pwrMode=** | Set up the Power Mode of a selected channel. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | | ||
+ | | **pwrMode?** | Displays the power mode for one selected DAC. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D. | | ||
+ | | **ldacMask=** | Set up the LDAC mask register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ set/reset mask:\\ 0 - reset LDAC mask for the selected channel.\\ 1 - set LDAC mask for the selected channel. | | ||
+ | | **ldacMask?** | Displays the LDAC register. | | ||
+ | | **intRef=** | Turns ON or OFF the internal reference. Accepted values:\\ 0 - turns OFF the internal reference.(default)\\ 1 - turns ON the internal reference. | | ||
+ | | **intRef?** | Displays the status of the internal reference. | | ||
+ | | **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | | ||
+ | | **ldacPin?** | Displays the value of LDAC pin. | | ||
- | **Section H** is used to control the Hardware pins of the AD7694R. | ||
- | **Section I** is used to perform a readback of all four registers of AD7694R. | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ :resources:fpga:xilinx:interposer:Terminal_KC705.jpg? }} | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board's user guide. | + | {{page>import_workspace}} |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//**. | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page>ez_common}} | {{page>ez_common}} |